• AVR Freaks

Hot!MPLAB X v5.10 'Power target circuit from ICD 3' doesn't work

Author
lightray
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/02/21 08:39:05
  • Location: 0
  • Status: offline
2019/02/22 11:18:24 (permalink)
0

MPLAB X v5.10 'Power target circuit from ICD 3' doesn't work

Hello,
 
Does anybody know how to fix this issue?
 
I enable 'power target circuit from ICD 3' from project properties -> ICD 3 -> Option categories: power.
 
But it always gives me below information.
 
Connecting to MPLAB ICD 3...
Currently loaded firmware on ICD 3
Firmware Suite Version.....01.54.00
Firmware type..............PIC32MX
Target device was not found (could not detect target voltage VDD). You must connect to a target device to use ICD3.
 
This option works fine in MPLAB X v3.**.
 
Thanks.
#1

4 Replies Related Threads

    domble
    Senior Member
    • Total Posts : 119
    • Reward points : 0
    • Joined: 2007/01/25 04:11:53
    • Location: 0
    • Status: offline
    Re: MPLAB X v5.10 'Power target circuit from ICD 3' doesn't work 2019/04/18 08:38:42 (permalink)
    0
    Just noticed the same myself; trying to program a PIC18F14K22, behaving as though target power was turned off although it was certainly on in project options.  Programmed fine with external power to the target.  And then programming a PIC32MX, the opposite - it said target power was on, although it was turned off in project options.
     
    I did have multiple projects open; on closing all projects and then re-opening the PIC18 one, target power option worked correctly again.  I generally have external power available anyway so I didn't pursue the issue further.
     
    Still using 5.10 until I see any great advantage in changing to 5.15.
     
    dom.
     
    #2
    qhb
    Superb Member
    • Total Posts : 9998
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: MPLAB X v5.10 'Power target circuit from ICD 3' doesn't work 2019/04/18 23:51:45 (permalink)
    0
    MPLABX does not seem to activate programmer power settings as soon as you change them, like MPLAB8 does.
    Often you have to exit MPLABX and start it again after changing a power setting before it activates.
     

    Nearly there...
    #3
    crosland
    Super Member
    • Total Posts : 1579
    • Reward points : 0
    • Joined: 2005/05/10 10:55:05
    • Location: Bucks, UK
    • Status: offline
    Re: MPLAB X v5.10 'Power target circuit from ICD 3' doesn't work 2019/04/19 01:34:47 (permalink)
    #4
    domble
    Senior Member
    • Total Posts : 119
    • Reward points : 0
    • Joined: 2007/01/25 04:11:53
    • Location: 0
    • Status: offline
    Re: MPLAB X v5.10 'Power target circuit from ICD 3' doesn't work 2019/05/14 03:41:15 (permalink)
    0
     I have three projects open, two on ICD3 (one's a bootloader) and one on PICkit3.  Hold in reset doesn't help here.  Every PICkit3 operation says 'Programmer to target power is enabled - VDD = 5.000000 volts.' although it is most certainly turned off in project properties (for all three projects).
    Just tried restarting MPLABX with only one project open - the power setting is still stuck at whatever it was at when mplabx was restarted. 
    Closing and reopening just the project (leaving mplabx running) does update the power setting.  
    Guess this is a new feature for 5.10, not tried 5.15 yet (super-slow office internet).
    #5
    Jump to:
    © 2019 APG vNext Commercial Version 4.5