• AVR Freaks

Hot!MPLAB HARMONY 2.06 INTERCAE WITH AR1021 TOUCH DRIVER

Author
AVR
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2016/09/26 01:35:50
  • Location: 0
  • Status: offline
2019/01/28 22:13:10 (permalink)
0

MPLAB HARMONY 2.06 INTERCAE WITH AR1021 TOUCH DRIVER

Hi ,
 
Is there any example project /code for interfacing AR1021 toch driver to MPLAB harmony 2.06 version.? New version of harmony (2.06 )says AR1021 driver is deprecated. 
 
Thanks and regards,
AVR
#1

2 Replies Related Threads

    jtzeng
    Super Member
    • Total Posts : 463
    • Reward points : 0
    • Joined: 2003/11/07 12:42:20
    • Status: offline
    Re: MPLAB HARMONY 2.06 INTERCAE WITH AR1021 TOUCH DRIVER 2019/01/28 23:48:25 (permalink)
    0
    The AR1021 was last supported in H1.XX.  It also has some errors in documentation and how it works.
    Most design in H2.06 for resistive touch have moved to the Touch_ADC driver which is a little more solid than the AR1021. 
    Is there a reason not to use the Touch_ADC?
     
     

    John Zigrang
    JTZ Engineering, Inc.
    #2
    AVR
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2016/09/26 01:35:50
    • Location: 0
    • Status: offline
    Re: MPLAB HARMONY 2.06 INTERCAE WITH AR1021 TOUCH DRIVER 2019/01/30 04:29:41 (permalink)
    0
    Hi John Zigrang,
     
    Thank you so much for your reply.
    In our last project we have used harmony 1.08 with AR1021 touch driver ,and was working satisfactorily.So we thought of using the same hardware with 2.06 version also.Now we have started our testing with ADC touch driver.
     
    Is there any document for how to use these deprecated drivers in 2.06 version?
     
    Regards,
    AVR
    #3
    Jump to:
    © 2019 APG vNext Commercial Version 4.5