• AVR Freaks

Hot!Atsama5d2 pin tool?

Author
balao
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2019/01/27 12:16:21
  • Location: 0
  • Status: offline
2019/01/27 22:37:04 (permalink)
0

Atsama5d2 pin tool?

Hi,

I like to ask is there any pin tool to MPU's 5d2 family.

I have ecad schema model of this individual chip, but the need paper size need to be something A3.

Or is the pinout table available e.g Excel format? I mean the pinout table, which shows the pin and signal names and powering groups in datasheet.
Even better if there is already available some ecad library with component units.

Thanks.
#1

0 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5