Hot!Supported packages for PIC24FJ128GA412

Author
perencia
New Member
  • Total Posts : 13
  • Reward points : 0
  • Joined: 2018/02/04 03:27:27
  • Location: 0
  • Status: offline
2019/01/11 02:47:47 (permalink)
0

Supported packages for PIC24FJ128GA412

Hello,
The last MCC version (3.66) supports the PIC24FJ128GA412 chip but the available packages shown on the Pin Manager are only TQFP128 and QFP128 whilst, according to the datasheet, that chip is only available in a 121-Pin TFBGA package.
Am I missing something?
#1

1 Reply Related Threads

    du00000001
    Just Some Member
    • Total Posts : 2498
    • Reward points : 0
    • Joined: 2016/05/03 13:52:42
    • Location: Germany
    • Status: offline
    Re: Supported packages for PIC24FJ128GA412 2019/01/11 05:54:18 (permalink)
    0
    I didn't check the datasheet...
    But if the packages differ only in the number of supply/ground pins, you might get away using the ?QFP128 scheme.
    Although the pin numbering won't match.

    PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5