Re: Snap. Failed to get Device ID
2019/01/08 14:00:21
(permalink)
When you can't get a deviceID, it typically means that there is a connection issue between the tool and the target. Make sure you have the PGC/PGD, MCLR, Vdd, and GND connected. Also make sure there is nothing else on the PGC/PGD lines or MCLR. You will not be able to do anything until you get a correct deviceID.
_____________________________
Please read the forum posting guidelines. Do not double post, please help keep these forums professional and comments respectful.
Please notify the moderators of problems/spam/trolls.