• AVR Freaks

Hot!Harmony V3 Came out?

Page: < 12 Showing page 2 of 2
Author
eclipse80
New Member
  • Total Posts : 18
  • Reward points : 0
  • Joined: 2016/03/06 10:16:00
  • Location: 0
  • Status: offline
Re: Harmony V3 Came out? 2019/03/23 20:43:09 (permalink)
0
Will they add PIC32MX support? Does anybody know?
post edited by eclipse80 - 2019/03/23 23:15:51
#21
JPortici
Super Member
  • Total Posts : 894
  • Reward points : 0
  • Joined: 2012/11/17 06:27:45
  • Location: Grappaland
  • Status: offline
Re: Harmony V3 Came out? 2019/03/24 00:47:36 (permalink)
0
HKPhysicist
I think Harmony 3 is already out for download, but is it good for production?  Smile: Smile
 
https://microchip-mplab-harmony.github.io/




i think it's as good for production as harmony 1 or 2 are ;)
#22
Tim Cruise
Junior Member
  • Total Posts : 94
  • Reward points : 0
  • Status: offline
Re: Harmony V3 Came out? 2019/03/24 04:33:10 (permalink)
0
eclipse80
Will they add PIC32MX support? Does anybody know?



For now, the supported MCUs are PIC32MK, PIC32MZ, Atmel ARM32.  PIC32MX is supported in Harmony v2.   mr green
#23
lelsteph
Super Member
  • Total Posts : 405
  • Reward points : 0
  • Joined: 2008/09/17 05:10:00
  • Location: 0
  • Status: offline
Re: Harmony V3 Came out? 2019/05/14 05:36:45 (permalink)
0
It seems CAN is not available in v3...
#24
arpananand
Super Member
  • Total Posts : 441
  • Reward points : 0
  • Joined: 2009/11/18 04:35:42
  • Location: 0
  • Status: offline
Re: Harmony V3 Came out? 2019/05/14 07:31:08 (permalink)
0
eclipse80
Will they add PIC32MX support? Does anybody know?


Some of the MX device support in H3 is coming soon.
#25
Kiku
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/05/06 15:48:11
  • Location: 0
  • Status: offline
Re: Harmony V3 Came out? 2019/08/06 07:24:30 (permalink)
0
Hello everyone
A few months ago I had to create a PCB with PIC32MK1024MCF100 to control 4 CAN BUS and I already noticed faults in harmony when I noticed that I only initialized two bus 1 and 4, I had to modify the starter boot of the ports to system_init. c ... I spent several days until I found the error, I have to say that I am new to MPLAB (1 year) since I used Mikroc but I think the support that can be given to us by the home software should be more big or better than secondary markers.
For now, a few days ago I started to develop USB to add to the 4 CAN bus device that works pretty well and I encounter all this, the problems of USB.
Do we know dates for a real USB support for PIC32MK?
I recently saw something in GitHub with CDC, but what about the rest?
Thank you all
#26
m4l490n
Senior Member
  • Total Posts : 123
  • Reward points : 0
  • Joined: 2010/06/15 22:21:39
  • Location: 0
  • Status: offline
Re: Harmony V3 Came out? 2019/08/13 09:54:52 (permalink)
0
arpananand
eclipse80
Will they add PIC32MX support? Does anybody know?


Some of the MX device support in H3 is coming soon.




There is support for PIC32MX. Last week I created a project for the PIC32MX795F512L using MHC 3. The thing is that is poorly documented and very new, so is safe to assume that it contains a lot of issues right now and I would not recommend it for new designs. I'm creating my project with MHC 2 to be "safer"
#27
Kiku
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2019/05/06 15:48:11
  • Location: 0
  • Status: offline
Re: Harmony V3 Came out? 2019/12/05 11:53:42 (permalink)
0
 

I remove the above, in harmony 3 everything was solved, I have not checked the 4 CAN bus but the USB.
At the moment it is giving good results 
 
grin: grin
#28
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5