• AVR Freaks

PIC32MZ2048EFXXXX and AN9 / AN10

Author
jtzeng
Super Member
  • Total Posts : 480
  • Reward points : 0
  • Joined: 2003/11/07 12:42:20
  • Status: offline
2018/12/10 07:30:37 (permalink)
0

PIC32MZ2048EFXXXX and AN9 / AN10

I am working on a project for resistive touch and the A/D I need are AN9 and AN10.
I have not been able to get AN9 and AN10 to give a READY after a global software edge trigger.
All other analog inputs I try, AN21, AN14, AN32 and AN33 all do.
This is setup on ADCCH7, the shared ADC.
I know that AN9 and AN10 have other options for use and the pins have other options as well.
What could be preventing conversion and READY indication?
I have been working on this in the Harmony forum as well.
 

John Zigrang
JTZ Engineering, Inc.
#1

8 Replies Related Threads

    Jump to:
    © 2020 APG vNext Commercial Version 4.5