Web_net_server example with sst26 sqi flash
Hi, I am using Mplab x IDE v5.0, harmony 2.04 and pic32mz2048efh144 in Pic 32 MZ Embedded Connectivity with Floating Point Unit (EF) Starter Kit. As you know web_net_server_nvm_mpfs working on nvm, but nvm has limited memory. That is why I want to use onboard sst26 flash as a memory. Also I want to use mpfsupload feature. In web_server_nvm_mpfs example, when I open the mpfsupload feature, it is not working and someones in forum says that mpfsupload feature can not work with nvm. On the other hand, when I try to use mpfsupload feature in web_net_server_nvm_mpfs example, it works correctly but again for limited memory. For using sqi flash properyl I checked a lot of thread and tried countless time. At below you can see the most related threads.
https://www.microchip.com...9931.aspx#105009 https://www.microchip.com...034451.aspx?high=sst26For checking, if sst26 works correctly, I tried sqi_fat example and everything seems correct. In my last try, I use these repos
https://bitbucket.org/eri...rmony-2.04/src/master/https://bitbucket.org/eri...s/src/master/ and the configuration those I gave you below( This is the same configuration at first of microchip forum links). After this point, sqi_fat example also not working and I am stuck at this point for about 3 weeks. Is there anyone who bumped into this issue before?
PS: Thanks to all support so far from @friesen @luca pascarella.
post edited by alimerido - 2018/12/04 01:18:01