Hot!Updating the gateway channel configuration in LoRa evaluation kit

Author
jobishjohn.mklm
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2018/08/08 08:23:47
  • Location: 0
  • Status: offline
2018/11/21 23:49:10 (permalink)
0

Updating the gateway channel configuration in LoRa evaluation kit

Hi,
 
We have purchased a LoRa evaluation kit (dv164140-1) which contains a gateway and two RN2483 motes. The mote successfully communicates with the gateway on the default frequency channels (868.1, 868.3, 868.5 MHz). We would like to add channels between (865-867MHz)
 
We could successfully add/configure the channel frequencies on RN 2483 devices to our required frequencies between (865-867MHz) using the LoRa development Suite software. But we are not able to do the same channel configuration on the gateway.  It will be a great help if someone could suggest us how to do this.
 
Thank you for your valuable time
 
Regards
Jobish John
 
#1

1 Reply Related Threads

    Poovai.L
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2019/02/10 23:06:20
    • Location: 0
    • Status: offline
    Re: Updating the gateway channel configuration in LoRa evaluation kit 2019/02/13 01:39:46 (permalink)
    0
    I have also same problem. Are you find any solution?
    #2
    Jump to:
    © 2019 APG vNext Commercial Version 4.5