kuku
Senior Member
- Total Posts : 145
- Reward points : 0
- Joined: 2012/03/03 08:05:54
- Location: 0
- Status: offline
dead snap
I try to recovery it via mplab but each time I get this result (picture). Device manager see snap as "Bossa program port (COM7)" What now?
Attached Image(s)
|
NKurzman
A Guy on the Net
- Total Posts : 19154
- Reward points : 0
- Joined: 2008/01/16 19:33:48
- Location: 0
- Status: online
Re: dead snap
2018/11/07 07:11:03
(permalink)
It says to contact customer support. That will require entering a support ticket.
|
prj
Super Member
- Total Posts : 218
- Reward points : 0
- Joined: 2009/12/01 14:35:45
- Location: 0
- Status: offline
Re: dead snap
2018/11/07 08:52:35
(permalink)
Please plug the Snap back in. Give it a few seconds. Bring up the recovery dialog again. This time leave the Snap plugged in regardless of what the recovery dialog instructs (so do not unplug it when it says to unplug it). Also, if you are seeing it as a COM port already in Device Manager, disregard the process for putting it into recovery mode (in that, the jumper and cable process). Please post the results (even if they are the same). Thanks.
post edited by prj - 2018/11/07 08:55:11
|
kuku
Senior Member
- Total Posts : 145
- Reward points : 0
- Joined: 2012/03/03 08:05:54
- Location: 0
- Status: offline
Re: dead snap
2018/11/07 09:18:21
(permalink)
NKurzman It says to contact customer support. That will require entering a support ticket.
heh... ;) I think that forum is more helpful :) @prj Without any unplug or J3 junction is a bit better. They found com port and try to restore firmware but stay at 34% of writing. In this situation, when I unplug USB then I get info with connection error. So I think that it live but wating for something.
post edited by kuku - 2018/11/07 09:25:09
Attached Image(s)
|
prj
Super Member
- Total Posts : 218
- Reward points : 0
- Joined: 2009/12/01 14:35:45
- Location: 0
- Status: offline
Re: dead snap
2018/11/07 09:42:07
(permalink)
How long was it sitting at 34%? It can be several minutes. After you unplugged it, and plugged it back in, how did it show up in Device Manager? Was it still the COM port? Thanks.
|
kuku
Senior Member
- Total Posts : 145
- Reward points : 0
- Joined: 2012/03/03 08:05:54
- Location: 0
- Status: offline
Re: dead snap
2018/11/07 09:51:42
(permalink)
At 34% stay about 5min. After this I get dialog box with error. In manager still is visible as COM port.
|
Jim Nickerson
User 452
- Total Posts : 6912
- Reward points : 0
- Joined: 2003/11/07 12:35:10
- Location: San Diego, CA
- Status: offline
Re: dead snap
2018/11/07 11:03:02
(permalink)
I wonder if it is plugged into USB 3 or 2 connector ? I wonder if it is plugged into connector on Hub or PC ? I wonder which OS you are running ?
|
kuku
Senior Member
- Total Posts : 145
- Reward points : 0
- Joined: 2012/03/03 08:05:54
- Location: 0
- Status: offline
Re: dead snap
2018/11/07 11:08:49
(permalink)
USB 2, direct to computer, win7 64bit. Last info who I see is "flash verify failed (-165)"
post edited by kuku - 2018/11/07 11:21:01
|
Jim Nickerson
User 452
- Total Posts : 6912
- Reward points : 0
- Joined: 2003/11/07 12:35:10
- Location: San Diego, CA
- Status: offline
Re: dead snap
2018/11/07 11:31:57
(permalink)
Sorry, I do not have a machine to try on. In some instances I have found changing to a different physical port has made a difference. Has it ever worked on this PC ?
|
kuku
Senior Member
- Total Posts : 145
- Reward points : 0
- Joined: 2012/03/03 08:05:54
- Location: 0
- Status: offline
Re: dead snap
2018/11/07 11:47:49
(permalink)
It's brand new but at start I have problem w driver instalation and I reinstal it. Next, Mplab not see snap so I try to recovery it....
|
DevMod1
Administrator
- Total Posts : 545
- Reward points : 0
- Joined: 2009/02/10 09:34:30
- Location: 0
- Status: offline
Re: dead snap
2018/11/08 10:20:39
(permalink)
Kuku, I have sent you a PM (private message) to have the Snap sent back for analysis and will get a new one out to you. Thanks,
_____________________________ Please read the forum posting guidelines. Do not double post, please help keep these forums professional and comments respectful. Please notify the moderators of problems/spam/trolls.
|
oliverb
Super Member
- Total Posts : 410
- Reward points : 0
- Joined: 2009/02/16 13:12:38
- Location: 0
- Status: offline
Re: dead snap
2018/12/06 02:00:50
(permalink)
I don't have experience with the SNAP but I have known USB devices that worked better with a hub between the device and PC.
|
Howard Long
Super Member
- Total Posts : 891
- Reward points : 0
- Joined: 2005/04/04 08:50:32
- Status: offline
Re: dead snap
2018/12/06 04:38:40
(permalink)
oliverb I don't have experience with the SNAP but I have known USB devices that worked better with a hub between the device and PC.
That is correct, some HS hubs and hosts have a limitation on multiple FS devices because they only have a single transaction translator. By adding an HS hub (or HS active extender) in between, it adds an additional transaction translator. Single TT hosts and hubs are a big headache and source of confusion if you try to support multiple FS devices on them!
|