swmcl
Super Member
- Total Posts : 277
- Reward points : 0
- Joined: 2014/05/10 13:54:42
- Location: Queensland
- Status: offline
ICD4 pinout
Hi, I am struggling as I think there is an issue with the User Guide for the ICD4. A response from a user with experience would be a little handy right now ... On DS50002596C-page 66 there is a representation of the RJ45 socket on the ICD4 in Figure B-2. The pinout shows pin1 at the bottom. If I take their cable and plug it into a RJ12 socket that I have then I do agree with their pictures on the right-hand side of Figure B-4. The table in Figure B-4 is upside down in that it should read as pins 1 to 6 and not 6 to 1 as I understand it. Pin1 was the reserved pin in Figure B-2. The table information in Figre B-3 is different also ... ! It lists pin1 to 6 but the information is again reversed. What do I believe ? What is the pinout of the RJ45 connector ? Is it pin1 at the bottom ? Given that I now have $250US worth of boards in process my enquiry may have come too late ... Rgds, Steve
|
NKurzman
A Guy on the Net
- Total Posts : 19144
- Reward points : 0
- Joined: 2008/01/16 19:33:48
- Location: 0
- Status: offline
Re: ICD4 pinout
2018/11/05 22:44:10
(permalink)
I think the issue maybe in the definition of the RJ45 cable. But it is easy enough to crimp one end backwards so you can use your boards.
|
Larry.Standage
Moderator
- Total Posts : 927
- Reward points : 0
- Joined: 2011/12/30 09:50:47
- Location: 0
- Status: offline
Re: ICD4 pinout
2018/11/06 09:08:43
(permalink)
The RJ45 connector has 8 pins, but the 6 critical ones are the inner six, so an RJ11 cable can be connected and have the correct pins. The two outer pins are used for JTAG debugging.
|
Jim Nickerson
User 452
- Total Posts : 6905
- Reward points : 0
- Joined: 2003/11/07 12:35:10
- Location: San Diego, CA
- Status: online
Re: ICD4 pinout
2018/11/06 09:19:07
(permalink)
Larry, I wonder if there is no danger that inserting the RJ11 plug will bend the outer RJ45 contacts so they will be difficult to use with a RJ45 plug in the future ? Or is the RJ45 receptacle on the ICD 4 special ?
|
NKurzman
A Guy on the Net
- Total Posts : 19144
- Reward points : 0
- Joined: 2008/01/16 19:33:48
- Location: 0
- Status: offline
Re: ICD4 pinout
2018/11/06 14:17:41
(permalink)
Well since I did not Notice they added 2 more pins to the ICD4, I guess not. The Microchip 6 inch 6X8 RJ-45 cable does not appear to damage the 2 extra pins. They are still all in a nice straight line.
|
swmcl
Super Member
- Total Posts : 277
- Reward points : 0
- Joined: 2014/05/10 13:54:42
- Location: Queensland
- Status: offline
Re: ICD4 pinout
2018/11/06 22:48:49
(permalink)
Respondees.. Could I ask for a pinout diagram of a socket on a board and the respective pins ? My technical enquiry at Microchip has them asking me to buy a Universal Programmer so that we can 'talk the same language' ... ! I have tested a low-resistance connection from pin 5 of their picture of the RJ45 in Figure B-4 to the ground of the external power port. This would indicate to me that their RJ45 picture is correct for at least one pin !
|
swmcl
Super Member
- Total Posts : 277
- Reward points : 0
- Joined: 2014/05/10 13:54:42
- Location: Queensland
- Status: offline
Re: ICD4 pinout
2018/11/06 22:49:42
(permalink)
Is there a way to test the pins with a scope in a 'live' kind of way before plugging it into a board ?
|
Jim Nickerson
User 452
- Total Posts : 6905
- Reward points : 0
- Joined: 2003/11/07 12:35:10
- Location: San Diego, CA
- Status: online
Re: ICD4 pinout
2018/11/07 08:03:09
(permalink)
swmcl Is there a way to test the pins with a scope in a 'live' kind of way before plugging it into a board ?
Maybe you could connect the included test board ?
|
swmcl
Super Member
- Total Posts : 277
- Reward points : 0
- Joined: 2014/05/10 13:54:42
- Location: Queensland
- Status: offline
Re: ICD4 pinout
2018/11/07 12:59:25
(permalink)
Hi Jim, Tried that ! The included test board is very sparse on detail and usability from that point of view. Tiny little vias with no markings. Given the money paid for the ICD4 they could supply a good breakout board for sure. Very poor service in my opinion. It would cost all of $2US on EBay if the Chinese were making and selling them ... Sadly, it looks as though I will have to just plug it in and see what happens. A lot of the pins out of the ICD4 are protected and I have poured over the User Guide (which I might say has been substantially edited in the last couple of weeks from the 'C' version to the 'D' version in this particular section ...) Cheers, Steve
|
qhb
Superb Member
- Total Posts : 9999
- Reward points : 0
- Joined: 2016/06/05 14:55:32
- Location: One step ahead...
- Status: offline
Re: ICD4 pinout
2018/11/07 14:16:08
(permalink)
It's a test board, not a "breakout" board. You connect it, and run the self test.
|
NKurzman
A Guy on the Net
- Total Posts : 19144
- Reward points : 0
- Joined: 2008/01/16 19:33:48
- Location: 0
- Status: offline
Re: ICD4 pinout
2018/11/07 15:37:03
(permalink)
|
swmcl
Super Member
- Total Posts : 277
- Reward points : 0
- Joined: 2014/05/10 13:54:42
- Location: Queensland
- Status: offline
Re: ICD4 pinout
2018/11/08 23:42:23
(permalink)
q ... it would be really inconvenient for Microchip to build the one board with a few well-labelled vias large enough for a probe I admit. Really, really inconvenient and costly. Thanks NK I'll check it out. The User Guide has undergone significant revision over the last few weeks (literally!) and the section pertaining to the pinouts is better but is still misleading in my view. The new boards are in flight with FedEx so I'll find out in a few days time I guess.
|