ICD3 "Initialization failed: Unable to create ControlPointMediator" connection error
Hi guys
I have installed my new PC, i've windows 10 pro 64 bit version.
I have installed MPLAB IDE v8.92 and MPLABX IDE v5.05.
Finally, I have open MPLAB driver switcher to set the ICD3 able to work with MPLAB X IDE.
When i have run MPLAB IPE tool, or MPLAB X IDE, and I have tried to connect to the ICD3, I couldn't open the connection to the tool.
The software tool has generated this message record:
"Initialization failed: Unable to create ControlPointMediator"
Instead, i use MPLAB driver switcher to set ICD3 able to work with MPLAB IDE, and when i have tried to connecto to the ICD3, it has worked correctly.
How can i use the ICD3 device with MPLAB X IDE and IPE softwares?