• AVR Freaks

Helpful ReplyADC Conversion Time Calculation in 12 bit operation dsPIC33EP512GM710

Author
joshua.cochran
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2018/09/25 07:40:46
  • Location: USA
  • Status: offline
2018/11/01 13:51:01 (permalink)
0

ADC Conversion Time Calculation in 12 bit operation dsPIC33EP512GM710

Hello all,
 
I am new to Microchip devices and I am using a dsPIC33EP512GM710 on a Explorer 16/32 development board to sample using an ADC at 12 bit resolution.
 
I would like to sample at 400 kHz, just shy of the maximum 500 kHz speed advertised by the board. I am using the internal clock for timing the ADC, and the internal counter ends sampling and starts conversion (SSRC = 7). 
 
My question:
The manual for the ADC for this microcontroller family states that "The ADC conversion time will be 12 TAD since the ADC module is configured for 10-bit operation, as calculated in Equation 16-9"
 
Is this true for 12 bit operation as well? Or is it 14 TAD?
#1
du00000001
Just Some Member
  • Total Posts : 4113
  • Reward points : 0
  • Joined: 2016/05/03 13:52:42
  • Location: Germany
  • Status: offline
Re: ADC Conversion Time Calculation in 12 bit operation dsPIC33EP512GM710 2018/11/01 14:01:57 (permalink)
0
I didn't check the data sheet (expect to find an equation for 12 bit conversions as well), but expect that 12 bit conversions take (at least) 2 TAD more than 10 bit conversions.
So 14 seems to be reasonable.

PEBKAC / EBKAC / POBCAK / PICNIC (eventually see en.wikipedia.org)
#2
jtemples
عُضْوٌ جَدِيد
  • Total Posts : 12032
  • Reward points : 0
  • Joined: 2004/02/13 12:31:19
  • Location: Southern California
  • Status: offline
Re: ADC Conversion Time Calculation in 12 bit operation dsPIC33EP512GM710 2018/11/01 14:04:07 (permalink) ☄ Helpfulby joshua.cochran 2018/11/01 17:20:18
5 (1)
Look at Table 33-59.
#3
joshua.cochran
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2018/09/25 07:40:46
  • Location: USA
  • Status: offline
Re: ADC Conversion Time Calculation in 12 bit operation dsPIC33EP512GM710 2018/11/01 17:24:24 (permalink)
0
Wow, thank you. I would have never found that table. I think I can work this out tomorrow using that table!
 
Also, do you know what the MCC (or compiler) defaults to if I have the ADC setup to run faster than possible?
 
For instance, the MCC only throws a warning telling me that TAD < minimum TAD of 11.76e-8s -- it still compiles and APPEARS to sample correctly even though I had TCY = 1, TAD = 1 with conversion clock source as FOSC/2.
#4
Jump to:
© 2021 APG vNext Commercial Version 4.5