Hot!THE big question, Standalone programming PC software? (NOT IPE!)

Page: < 12 Showing page 2 of 2
Author
MBedder
Circuit breaker
  • Total Posts : 6697
  • Reward points : 0
  • Joined: 2008/05/30 11:24:01
  • Location: Zelenograd, Russia
  • Status: offline
Re: THE big question, Standalone programming PC software? (NOT IPE!) 2019/01/18 16:09:29 (permalink)
0
Or
 
7) Buy out the competitors to make sure their products can't be programmed without troubles
#21
crosland
Super Member
  • Total Posts : 1525
  • Reward points : 0
  • Joined: 2005/05/10 10:55:05
  • Location: Bucks, UK
  • Status: offline
Re: THE big question, Standalone programming PC software? (NOT IPE!) 2019/01/19 02:57:06 (permalink)
0
malaugh
One suggestion is to use the command line executable ipecmd.  We use this in a batch file to automate our factory programming procedure.  Much easier for unskilled workers than using IPE and having to selecting the correct CPU and image file EVERY TIME YOU USES THE PROGRAM.
 
We currently use ICD3s, and I am not sure if this program was updated to use an ICD4.  


Another suggestion would be to use production grade programmers in a production environment.
 
Sorry, seems the ICD3 IS a production grade programmer. I am surprised at that.
post edited by crosland - 2019/01/20 09:29:14
#22
Page: < 12 Showing page 2 of 2
Jump to:
© 2019 APG vNext Commercial Version 4.5