• AVR Freaks

Looking for link to documentation for configuring secondary oscillator for PIC16F1619

Author
meyerjoh
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2016/07/15 14:33:40
  • Location: 0
  • Status: offline
2018/10/26 16:28:49 (permalink)
0

Looking for link to documentation for configuring secondary oscillator for PIC16F1619

Dear Experts,
 
I am hoping to use the timer 1 interrupt to wake a 8 bit PIC from sleep. It is my understanding that the secondary oscillator will continue oscillating through sleep. However, I have not been able to find any documentation on how the secondary oscillator is configured and/or enabled. Even the PIC16F1619 (for instance) only has four instances of the word "secondary", and none of them near any configuration information.
 
I'm sure that there has to be some information, perhaps in an application note somewhere!
 
Any help/advice would be much appreciated!
#1

3 Replies Related Threads

    qhb
    Superb Member
    • Total Posts : 9999
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: Looking for link to documentation for configuring secondary oscillator for PIC16F1619 2018/10/26 16:45:01 (permalink)
    +1 (1)
    I don't believe the PIC16F1619 has a secondary oscillator.
    The occasional use of the word "secondary" will be an accidental cut&paste from another datasheet.
    Your only alternative is to use the WDT to wake up from sleep.
     

    Nearly there...
    #2
    QuiqueG
    Super Member
    • Total Posts : 122
    • Reward points : 0
    • Joined: 2010/09/01 12:35:40
    • Location: DM43BH
    • Status: offline
    Re: Looking for link to documentation for configuring secondary oscillator for PIC16F1619 2018/10/28 22:38:25 (permalink)
    +1 (1)
     
    Section 22.7 of the datasheet describes the use of Timer1 during sleep in order to wake up the device.  The timer needs to run in async counter mode.
     
    #3
    qhb
    Superb Member
    • Total Posts : 9999
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: Looking for link to documentation for configuring secondary oscillator for PIC16F1619 2018/10/28 22:39:36 (permalink)
    +1 (1)
    "asynch counter mode" means you need an external clock input.

    Nearly there...
    #4
    Jump to:
    © 2021 APG vNext Commercial Version 4.5