• AVR Freaks

Hot!USB2642 - Where is USBDM installed in Windows 10?

Author
f.ch
New Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2018/01/31 11:53:19
  • Location: 0
  • Status: offline
2018/10/25 12:38:57 (permalink)
0

USB2642 - Where is USBDM installed in Windows 10?

Hi,
 
I downloaded the USBDM tool from the USB2642 page and installed it, but I can't find where it was installed. In the user guide, it says that we can use it by clicking on "Start\Programs\USBDM\USBDM icon", but I can't find it. It's not in Program Files or Program Files (x86). I used the x64 installer.
 
Where is it?
 
Thank you,
 
Fred
 
#1

2 Replies Related Threads

    f.ch
    New Member
    • Total Posts : 15
    • Reward points : 0
    • Joined: 2018/01/31 11:53:19
    • Location: 0
    • Status: offline
    Re: USB2642 - Where is USBDM installed in Windows 10? 2018/10/25 16:35:35 (permalink)
    +1 (3)
    Nevermind, I found it by searching "usbdm" here: https://www.microchip.com/technical-support/hot-topics
     
    "Note: On a Windows 8 machine you can find the installed exe in C:\ProgramData\Microsoft\Windows\Start Menu\Programs\USBDM\USBDM.exe"
     
    It's the same on Windows 10
    #2
    sh_azmoodeh
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2020/03/27 06:46:46
    • Location: 0
    • Status: offline
    Re: USB2642 - Where is USBDM installed in Windows 10? 2020/03/29 02:28:42 (permalink)
    0
    Also i have this.
    in windows 10 USBDM not found on startmenu or this location. its seems absolutely not installed.
    #3
    Jump to:
    © 2021 APG vNext Commercial Version 4.5