• AVR Freaks

AnsweredHot!Installing the AVR toolchain for use on MPLAB X IDE

Author
vleroylr
Starting Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2018/08/09 20:12:20
  • Location: 0
  • Status: offline
2018/10/20 22:32:46 (permalink)
0

Installing the AVR toolchain for use on MPLAB X IDE

Hi, I wanted to know how to install the AVR tool chain so I can write code inside MPLAB X IDE the same I do in Atmel Studio to later compile and program the device with my Atmel Ice. I tried installing the tool chain (https://www.microchip.com...oolchains-c-compilers) and then put the install location on "add" from the toolchain menu on options/embedded inside mplab X, but never worked... so any help would be very appreciated.
#1
hkv
Starting Member
  • Total Posts : 15
  • Reward points : 0
  • Joined: 2018/08/06 10:11:49
  • Location: 0
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2018/11/09 11:42:33 (permalink)
0
On choosing the directory and adding it, the bin folder directory's address is the one that should be used.
#2
RISC
Super Member
  • Total Posts : 5585
  • Reward points : 0
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2018/11/09 14:56:25 (permalink) ☼ Best Answerby vleroylr 2018/11/16 06:07:57
+1 (3)
Hi,
 
Do you want to compile code for 8bits AVRs ?
If so, just install XC8 v2.xx, it includes both PIC and AVR compilers
 
Regards
 
#3
vleroylr
Starting Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2018/08/09 20:12:20
  • Location: 0
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2018/11/16 06:09:22 (permalink)
0
Thanks for all of your responses,
 
And yes, I want to compile to 8 Bit AVR MCUs, is there any major difference between using XC8 and the compiler used in atmel studio?
I will try and use XC8, if anything goes strange I will be posting!, thanks again.
#4
fperal
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2008/11/25 03:57:09
  • Location: 0
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2018/12/28 17:25:43 (permalink)
+1 (1)
I'm trying to program in assembler AVR.
I downloaded the toolchain from AVR 8-bit Toolchain 3.6.2 - Linux 64-bit  and added it to mplabX in Tools-options.embeded.build tools-add. MPlabx recognizes it as AVR 5.4.0 and mark the tool green (full support). I have created a new project with standalone project and using the AVR toolchain, but every single program I try to compile reports errors.
 
 
#5
qhb
Superb Member
  • Total Posts : 9999
  • Reward points : 0
  • Joined: 2016/06/05 14:55:32
  • Location: One step ahead...
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2018/12/28 18:58:35 (permalink)
0
Sorry, can't quite make out what the errors say on your screen.
 

Nearly there...
#6
crosland
Super Member
  • Total Posts : 1937
  • Reward points : 0
  • Joined: 2005/05/10 10:55:05
  • Location: Warks, UK
  • Status: online
Re: Installing the AVR toolchain for use on MPLAB X IDE 2018/12/29 05:18:09 (permalink)
0
Do you have a question, or are you just telling us about your experience?
#7
Marek1914
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2018/01/12 00:26:23
  • Location: 0
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2019/02/11 11:41:57 (permalink)
0
I've  encountered the same issue!
Attachments are not available: Download requirements not met
 look: the same AVR code compiled with XC
 
Where should I look for the mistake?Any tricks/ suggestions with AVR tool chain adding in embedded build tools?Thanks for advice/ response...
post edited by Marek1914 - 2019/02/12 23:06:11

Attachment(s)

Attachments are not available: Download requirements not met
#8
DungeonLords
New Member
  • Total Posts : 9
  • Reward points : 0
  • Joined: 2019/05/05 08:41:21
  • Location: 0
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2019/09/02 03:59:47 (permalink)
0
This is my path to add avr-gcc 9.1 from http://blog.zakkemble.net/avr-gcc-builds/

Attachment(s)

Attachments are not available: Download requirements not met
#9
sn4tch3r
Starting Member
  • Total Posts : 32
  • Reward points : 0
  • Joined: 2011/07/06 04:08:27
  • Location: India
  • Status: offline
Re: Installing the AVR toolchain for use on MPLAB X IDE 2019/10/21 08:08:12 (permalink)
0

I am trying to import an Atmel Studio (AS7) Project based on AVR-GCC compiler on Linux Ubuntu18.04.3 LTS.
My toolchain on MPLAB X is AVR_GCC version 5.4.0 provided by Microchip Site. I would want to stick to AVR_GCC since my entire project has been maintained on this compiler. 
I have successfully performed this task of transition from AS7 to MPLAB-X on Windows 10.
My problem is transition from Windows to Linux where I am having this issue which states that AVR (v1.0.0) isn't supported.
My existing code has loads of issues when used with xc8 compiler, especially related to strings and pointers.
 
I have tried using the default location at /usr/bin too which again prompts the same problem.
What do I do ?

Regards,
Nelson Lobo
#10
Jump to:
© 2020 APG vNext Commercial Version 4.5