• AVR Freaks

USB CDC serial emulator communication issue

Author
Taj mohammad
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2018/10/10 22:39:40
  • Location: 0
  • Status: offline
2018/10/13 02:42:12 (permalink)
0

USB CDC serial emulator communication issue

Hi, I am using PIC32MZ2048ECH144 and MPLAB X IDE with harmony configurator. working on CDC serial emulator demo. I am not using PIC32 evaluation board. I used software pull ups for device detection. Configured the device in USB full speed mode.Added apps.c and apps.h files from cdc serial emulator of PIC32MX demo code. Installed the device driver through .INF folder. Now the device is being detected and COM port is allotted. The demo code should echo the received data. But it is not happening while i am sending.
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5