Re: BM71 command 0x39 always fail
2018/10/13 02:57:11
(permalink)
Update: Finally solved this problem, the solution is, one have to check the "attribute updated" check box when creating Characteristics in configuration tool to allow 0x39 operates! Now only if someone can point to me, in which document do this behavior well documented, so that next time I (or somebody else) will not again make such mistake anymore?