Hot!Can't program PIC18F46K80 using PICKIT 4.

Author
eugen1995
New Member
  • Total Posts : 3
  • Reward points : 0
  • Joined: 2018/10/10 05:25:32
  • Location: 0
  • Status: offline
2018/10/10 23:51:21 (permalink)
0

Can't program PIC18F46K80 using PICKIT 4.

    Hello, i can't program PIC18F46K80 using PICKIT 4 and MPLAB X v5.05. Device ID can't be read. But i can program same board using PICKIT3. I managed to program different board with PIC18F2480 on it using PICKIT 4, so there is not a problem with PICKIT 4 programmer. I there something else i can try to do? 
     One thing i am guessing that PIC18F46K80  still has beta support and thats why i cant program it... Can it be true? 
 
#1

5 Replies Related Threads

    Jim Nickerson
    User 452
    • Total Posts : 5812
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Can't program PIC18F46K80 using PICKIT 4. 2018/10/11 06:14:46 (permalink)
    0
    I wonder what it says in
    C:\Program Files (x86)\Microchip\MPLABX\v5.05\docs\Device Support.htm
    ?
    #2
    eugen1995
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2018/10/10 05:25:32
    • Location: 0
    • Status: offline
    Re: Can't program PIC18F46K80 using PICKIT 4. 2018/10/11 06:29:08 (permalink)
    3 (1)
    It says, that that PIC18F46K80 and PIC18F2480 both have a preliminary, beta support - yellow mark. But there 90% of PICKIT4 devices have yellow mark. And PICKIT 3 have almost all green - production tested support. So i am guessing that for now PICKIT 4 is pretty useless???
    #3
    Jim Nickerson
    User 452
    • Total Posts : 5812
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: offline
    Re: Can't program PIC18F46K80 using PICKIT 4. 2018/10/11 06:31:26 (permalink)
    0
    The price we pay for being on the "Bleeding Edge" ?
    #4
    DevMod1
    Administrator
    • Total Posts : 434
    • Reward points : 0
    • Joined: 2009/02/10 09:34:30
    • Location: 0
    • Status: offline
    Re: Can't program PIC18F46K80 using PICKIT 4. 2018/10/11 09:48:34 (permalink)
    4 (1)
    Have you tried to slow down the programming in the tools properly page??  The PICkit 4 is much faster than PICkit 3.

    _____________________________

    Please read the forum posting guidelines. Do not double post, please help keep these forums professional and comments respectful.
    Please notify the moderators of problems/spam/trolls.
    #5
    eugen1995
    New Member
    • Total Posts : 3
    • Reward points : 0
    • Joined: 2018/10/10 05:25:32
    • Location: 0
    • Status: offline
    Re: Can't program PIC18F46K80 using PICKIT 4. 2018/10/12 05:20:57 (permalink)
    5 (1)
    DevMod1
    Have you tried to slow down the programming in the tools properly page??  The PICkit 4 is much faster than PICkit 3.


    Yeah, i tried to change program speed from normal to slow, but no luck. Still i would get the same error.
    #6
    Jump to:
    © 2019 APG vNext Commercial Version 4.5