• AVR Freaks

Boot Loader for PIC18F57K42

Author
ashasingh18
Starting Member
  • Total Posts : 55
  • Reward points : 0
  • Joined: 2018/05/17 18:06:09
  • Location: 0
  • Status: offline
2018/10/09 13:32:32 (permalink)
0

Boot Loader for PIC18F57K42

Hi,
I had asked about generating a boot loader for our product with PIC18F57K42 back couple of months and 
was pointed towards using MCC to generate the code for my boot loader.  However, at that time, the MCC 
had limitation on supporting this chip because this PIC18F57K42  was too big -- 128K
I was wondering if a new MCC has been released that can support generating code for PIC18F57K42?
 
The MCC  Core v4.45 is what I have.
Thanks,
Asha
 
#1

5 Replies Related Threads

    katela
    Super Member
    • Total Posts : 1947
    • Reward points : 0
    • Joined: 2013/06/11 05:25:18
    • Location: South Africa
    • Status: offline
    Re: Boot Loader for PIC18F57K42 2018/10/09 14:19:18 (permalink)
    0
    That kind of information could be in the new MCC release note.

    Free online Microcontroller Tutorials and Projects for Hobbyists and students. From beginners to advanced. Website: www.studentcompanion.co.za
    YouTube Tutorials: https://www.youtube.com/StudentCompanionSA
    #2
    Danno
    Super Member
    • Total Posts : 289
    • Reward points : 0
    • Joined: 2005/09/07 10:12:10
    • Status: offline
    Re: Boot Loader for PIC18F57K42 2018/10/09 15:18:34 (permalink)
    +1 (1)
    A new release of the MCC bootloader has been posted to www.microchip.com/mcc.  It half fixes the 7K42 128KB problem.  The main reason for the release was to update the generated code for C99 compatibility.  Also to fix the memory corruption issue for PIC16F1's when using the lower optimization levels. 
     
    The 24 bit length has been implemented on the checksum command, however the host side has not been updated to take advantage.  It's still red lit for those devices :-(   
     
    See the release notes at the same website FMI.
     
    Sorry, this update was to the generated firmware only.
    #3
    ashasingh18
    Starting Member
    • Total Posts : 55
    • Reward points : 0
    • Joined: 2018/05/17 18:06:09
    • Location: 0
    • Status: offline
    Re: Boot Loader for PIC18F57K42 2018/10/09 15:24:51 (permalink)
    0
    Hi,
    Thank you for this info.  I tried to get to the release notes but could not find it.
    Thanks,
    Asha
    #4
    qhb
    Superb Member
    • Total Posts : 9999
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: Boot Loader for PIC18F57K42 2018/10/09 15:30:01 (permalink)
    +1 (1)
    ashasingh18
    Thank you for this info.  I tried to get to the release notes but could not find it.

    If you go to https://www.microchip.com/mplab/mplab-code-configurator
    select the "Current download" tab, and the "release notes" link is right next to the "download" link.
    Scroll down to "8 bit bootloader", and the link goes to:
    http://ww1.microchip.com/downloads/en/DeviceDoc/bootloader8bit_v2.2.37_Release%20Notes.pdf
     

    Nearly there...
    #5
    ashasingh18
    Starting Member
    • Total Posts : 55
    • Reward points : 0
    • Joined: 2018/05/17 18:06:09
    • Location: 0
    • Status: offline
    Re: Boot Loader for PIC18F57K42 2018/10/09 15:37:25 (permalink)
    0
    Hi,
    Thank you, 
    Got the release note for the boot loader.
    Thanks,
    Asha
    #6
    Jump to:
    © 2021 APG vNext Commercial Version 4.5