Hot!Curiosity MX470 HID single touch example

Author
georgeLeung
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2018/10/03 23:42:39
  • Location: 0
  • Status: offline
2018/10/08 01:45:22 (permalink)
0

Curiosity MX470 HID single touch example

Hi,
 
I just got a Curiosity MX470 dev kit and need to work on a HID single touch device. I have downloaded harmony v2_06 but found that the HID example did not work on Curiosity MX470 right now. The example works on this board is the cdc com port. Could anyone provide a guideline such that I can port the HID single touch driver to that cdc com port project.
post edited by georgeLeung - 2018/10/08 01:46:29
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5