Hot!Read and Write i2C PCF8574 chip

Author
donpantof
New Member
  • Total Posts : 19
  • Reward points : 0
  • Joined: 2013/06/26 00:29:46
  • Location: 0
  • Status: offline
2018/10/04 01:35:13 (permalink)
0

Read and Write i2C PCF8574 chip

Hi,
I have connected over I2C bus a I2C-IN830M0 expander and a PIC32MX795F512L microcontroller. I2C-IN830M0 expander uses a PCF8574 I2C chip. For developing i used MPLAB x IDE v4.20. I want to read or write some addresses of expander. How can i do that? I've trying something, but  it doesn't work.... I used functions for reading and writing from pic I2c lib, functions like: MasterWriteI2C1, MasterReadI2C1. Can someone send me an working example that read and write one address of expander?
Thanks!
#1

9 Replies Related Threads

    qhb
    Superb Member
    • Total Posts : 9165
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: online
    Re: Read and Write i2C PCF8574 chip 2018/10/04 01:54:59 (permalink)
    +1 (1)
    You're unlikely to get someone to write some custom code just for you.
    Why not show us the actual code you tried, rather than just describing it in vague terms?
     
    #2
    donpantof
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2013/06/26 00:29:46
    • Location: 0
    • Status: offline
    Re: Read and Write i2C PCF8574 chip 2018/10/04 03:11:13 (permalink)
    0
    Hi,
    I cant send u entire code, but i send u this sample:
    //is my attempt to read
    //#define I2C_ADD   (0x27) // expander I2C address
     
           unsigned char i2cbyte;
          
            StartI2C1();       
            IdleI2C1();        
            MasterWriteI2C1((I2C_ADD << 1) | 1);
            IdleI2C1();      
           
    // I do not know if it's the correct address '0x41'
            MasterWriteI2C1(0x41);
            IdleI2C1();
           
            i2cbyte = MasterReadI2C1();    

            StopI2C1();       
            IdleI2C1();        
            
           printf("\ni2cbyte: %u\n", i2cbyte); // i want to display value that i read
     
    OBS: I forgot to tell u, but i connected a push button on  + IN1, - IN1 of expander and that is what i want to read, if button was pressed or not.
    OBS2: Jumpers ( A0, A1, A2 ) of expander board are close.
    OBS3:  It display value 255, even if button is pressed or not.
     
    P.S. I attached u a link: https://www.ereshop.com/s...e/I2C-IN830M_SHEET.pdf
          On page 5/7, Figure7: Addressing, i used address 0x41, i thought that is what i need.
     
    #3
    qhb
    Superb Member
    • Total Posts : 9165
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: online
    Re: Read and Write i2C PCF8574 chip 2018/10/04 04:32:50 (permalink)
    +1 (1)
    I haven't used those library functions, so not sure if you're using them correctly, but your I2C addressing is certainly wrong.
    You should be using 0x41 as the "I2C_ADD" value, not 0x27.
    You can only send one address after the START cycle, the very next cycle should be a read.
    That library should give you some way to check if the Slave sent an ACK pulse after the slave address has been sent.
     
    #4
    donpantof
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2013/06/26 00:29:46
    • Location: 0
    • Status: offline
    Re: Read and Write i2C PCF8574 chip 2018/10/09 01:00:41 (permalink)
    0
    Hi,
    I found another demo, just for reading, but it doesn't work either. Do u have any suggestions?
     
     I2CStart(I2C1);      
    while ( !(I2CGetStatus(I2C1) & I2C_START) );     
    I2CSendByte(I2C1, 0x41);     
    while(!I2CTransmissionHasCompleted(I2C1));     
    if(I2CByteWasAcknowledged(I2C1) && I2CReceiverEnable(I2C1, TRUE) != I2C_RECEIVE_OVERFLOW)     
    {           
         while(!I2CReceivedDataIsAvailable(I2C1));           
        I2CAcknowledgeByte (I2C1, TRUE);           
        i2cbyte = I2CGetByte(I2C1);
        while( !I2CAcknowledgeHasCompleted(I2C1));     
    }     
    else                              
         i2cbyte = 0xff;     
    I2CStop(I2C1);

     
     
    PS: Always value from i2cbyte  is 255 and it doesn't enter in else state.
    post edited by donpantof - 2018/10/09 01:26:17
    #5
    Antipodean
    Super Member
    • Total Posts : 1690
    • Reward points : 0
    • Joined: 2008/12/09 10:19:08
    • Location: Didcot, United Kingdom
    • Status: offline
    Re: Read and Write i2C PCF8574 chip 2018/10/09 08:18:38 (permalink)
    0
    Is your chip a PCF8574 or a PCF8574A. They have different address ranges - check the data sheet.
     

    Do not use my alias in your message body when replying, your message will disappear ...

    Alan
    #6
    donpantof
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2013/06/26 00:29:46
    • Location: 0
    • Status: offline
    Re: Read and Write i2C PCF8574 chip 2018/10/10 00:33:06 (permalink)
    0
    Hi,
    My chip is PCF8574, but never mind, i solved it. It works! Thanks!
    #7
    qhb
    Superb Member
    • Total Posts : 9165
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: online
    Re: Read and Write i2C PCF8574 chip 2018/10/10 05:24:43 (permalink)
    +1 (1)
    It's good manners to mention what the problem was, so anyone coming along later with the same problem can see where they may have gone wrong.
     
    #8
    donpantof
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2013/06/26 00:29:46
    • Location: 0
    • Status: offline
    Re: Read and Write i2C PCF8574 chip 2018/10/10 23:19:09 (permalink)
    +1 (1)
    I solved and it works! The code lines for reading are the same, i have not changed them. 
    It was a hardware error, witch i missed it. Like i said before, i connected a push button on  + IN1, - IN1 of expander, but i forgot to power it up.
    #9
    donpantof
    New Member
    • Total Posts : 19
    • Reward points : 0
    • Joined: 2013/06/26 00:29:46
    • Location: 0
    • Status: offline
    Re: Read and Write i2C PCF8574 chip 2018/10/10 23:19:24 (permalink)
    0
    Sorry! You are totally right! 
     
     
    #10
    Jump to:
    © 2019 APG vNext Commercial Version 4.5