DSPIC33EP - ICSP Pin
Dear All,
for the first time I wuld like to use in one of my new projects a dsPIC33EP32MC202.
In the datasheet I read that it can be programmed with the ICD3 interface (which I already have) and that in particular:
-ICSPCLK of ICD3 must be connected to a PGECx pin of the microcontroller
-ICSPDAT of ICD3 must be connected to a PGEDx pin of the microcontroller
What I don't understand is why there are several couples of PGEC-PGED pins on the microcontroller.
Are they all equivalent? Can I choose the couple of pin that for me are the best?
Thank you in advance,
Mattia