Re: help need for enable https
2018/09/20 22:33:09
(permalink)
thanks for the replay.
i am using the tcp ip client demo application, in that enabling the wolfssl will give me the https url access.
is that right? or do i need to do any additional settings or any api call need to be added in the code.
for setting the correct time, is enabling the sntp will give time correct? .
regd. wolfssl do i need to buy any licence?
please guide me.