• AVR Freaks

PIC32MZ I2C delay

Page: < 12 Showing page 2 of 2
Author
qhb
Superb Member
  • Total Posts : 9999
  • Reward points : 0
  • Joined: 2016/06/05 14:55:32
  • Location: One step ahead...
  • Status: offline
Re: PIC32MZ I2C delay 2018/10/17 12:36:01 (permalink)
0
AaronHancock
I gave up on the Harmony I2C and SPI drivers and wrote my own bit bang implementation.  I use timer delays to control the clock speed.  Not the most CPU time efficient way of doing things, but it is hard to argue with something that works.

Which the post before yours explains is already built in to Harmony. It contains a full "bit bang" implementation to do it for you.
 

Nearly there...
#21
Page: < 12 Showing page 2 of 2
Jump to:
© 2021 APG vNext Commercial Version 4.5