• AVR Freaks

RN-42-EK Software Version/Upgrade

Author
dylan0806
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2017/12/03 07:15:25
  • Location: 0
  • Status: offline
2018/09/11 02:14:48 (permalink)
0

RN-42-EK Software Version/Upgrade

Hi all,
 
Since I can't get a SPP connection working with a ATBTLC1000ZR I want to use a RN-42-I/RM.
Now I want to buy a RN-42-EK as a development board but want to use the new 6.30 firmware but how do I know if the RN-42-EK comes with version 6.30? Or is there a way to upgrade the software? I've got a JTAG Programmer (ATMEL ICE) and some usb to serial converters (FT232).
 
Tnx
#1

1 Reply Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 19144
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: RN-42-EK Software Version/Upgrade 2018/09/11 05:18:06 (permalink)
    0
    It appears to have a usb to serial converter on it. If it is the same as the 77 and 78 modules the update will connect via that. You will need to jumper the mode pins to put it in to flash mode.
    #2
    Jump to:
    © 2021 APG vNext Commercial Version 4.5