• AVR Freaks

Hi-Tech Z80 C compiler

Author
oldtimer
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2018/09/03 10:22:09
  • Location: 0
  • Status: offline
2018/09/05 07:09:48 (permalink)
0

Hi-Tech Z80 C compiler

Hi
 
I have a complete 1989 vintage Hi-Tech Z80 compiler (V4.11). Complete with origional 3 ring binder, hard copy manual and 5.5inch floppy disks.  As far as I can tell this only runs on 32 bit PC's (in a dos box) and won't run even in compatibility mode on a 64 bit system. 
 
As Microchip bought Hi-Tech and about  a decade ago stopped all the non-Pic Hi-Tech compilers:  can I make the Hi-Tech Z80 compiler available as on another  Z80 forum for other non-commercial/hobby developers? 
 
#1

10 Replies Related Threads

    NKurzman
    A Guy on the Net
    • Total Posts : 19192
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 08:50:28 (permalink)
    +1 (1)
    It is unlikely. But you can Ask.  Try a Support Ticket to start.
    It will still be under Copyright, so it is not free or open.
     
    #2
    oldtimer
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/09/03 10:22:09
    • Location: 0
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 08:58:31 (permalink)
    +1 (1)
    I agree, although Microchip removed the non-Pic Hi-Tech  compilers immediately and support for them as soon as possible in 2009 the rights to the compiler are still owned my Microchip.  
     
    No one is going to do anything commercial with it and most of the Z80 enthusiasts are all retired hobby people.
     
    I will try a support ticket  but I think that no one at the support level will have the authority to say anything other than "no!" :-(  
    #3
    NKurzman
    A Guy on the Net
    • Total Posts : 19192
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 09:14:31 (permalink)
    +2 (2)
    No they will not have a clue, but you can try to get them to push it to legal.  It may be your only choice unless you know an F.A.E.  If what you are looking to distribute is a free or sample version it will be easier. But if you are giving a key code it may be harder.
    #4
    oldtimer
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/09/03 10:22:09
    • Location: 0
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 09:41:23 (permalink)
    0
    There is no key code.  No licence management or activation system at all.  just the files most .exe but some .com
     
    It is a 16/32 bit DOS compiler from 1989.  It comes on 2 floppy disks and assumes you will be working on a PC with maybe the luxury of a second floppy disk (no hard disk at all unless you were a Power user)
     
    It really is from a different Millennium :-) I think it was obsolete and discontinued by Hi-tech long before Microchip bought them. 
     
    The only other commercial Z80 compiler I know is the IAR EW Z80 and that runs on Win7 but was also discontinued. About 5 years ago I think. I have that too but it is licensed (to me).
     
     
     
    #5
    Jim Nickerson
    User 452
    • Total Posts : 6933
    • Reward points : 0
    • Joined: 2003/11/07 12:35:10
    • Location: San Diego, CA
    • Status: online
    Re: Hi-Tech Z80 C compiler 2018/09/05 09:45:42 (permalink)
    +1 (1)
    This is interesting http://www.z80.eu/c-compiler.html
    #6
    JorgeF
    Super Member
    • Total Posts : 3345
    • Reward points : 0
    • Joined: 2011/07/09 11:56:58
    • Location: PT/EU @ Third rock from the Sun
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 10:23:12 (permalink)
    0
    Hi
    JANickerson
    This is interesting http://www.z80.eu/c-compiler.html

    It brings back some memories, from when I started with Pascal on top of CP/M on a TRS-80 Model II.
    @oldtimer: Only one single side 8" floppy drive.

    Best regards
    Jorge
     
    I'm here http://picforum.ric323.com too!
    And it works better....
    #7
    oldtimer
    New Member
    • Total Posts : 4
    • Reward points : 0
    • Joined: 2018/09/03 10:22:09
    • Location: 0
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 10:59:08 (permalink)
    0
    JorgeF
    It brings back some memories, from when I started with Pascal on top of CP/M on a TRS-80 Model II.
    @oldtimer: Only one single side 8" floppy drive.

    When mentioning "only a single floppy drive"   anyone under 50 assumes you also had a hard drive.... :-)
    and if you say  "5 inch disk" some people think you mean a CD!
     
    I can remember when CD drives (not DVD) were "new" and expensive. Now it seems with all SW being downloaded even the optical drives have gone from most computers.   I have CD/DVD drives and an external 3.25 floppy drive.  the problem is most new PC Bios will not recognise a floppy drive.  I keep a couple of old PC's and an Old Laptop so I can use some of the older SW and tools.
    #8
    PStechPaul
    Super Member
    • Total Posts : 3047
    • Reward points : 0
    • Joined: 2006/06/27 16:11:32
    • Location: Cockeysville, MD, USA
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 19:16:11 (permalink)
    0
    There may be other options for a Z80 compiler. I have done a lot of work on a Z-world "Smart Core" which has a Z180, using their "Dynamic C", but is now owned by Rabbit, or their successor, Digi International. Some links:
     
    https://www.z88dk.org/forum/
    https://github.com/z88dk
    https://www.digi.com/supp.t/productdetail?pid=4978
    http://sdcc.sourceforge.net/
    http://www.z80.info/z80sdt.htm
    https://www.bdsoft.com/resources/bdsc.html
    http://techtinkering.com/...80-c-compiler-for-cpm/

     
    #9
    qhb
    Superb Member
    • Total Posts : 9999
    • Reward points : 0
    • Joined: 2016/06/05 14:55:32
    • Location: One step ahead...
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/05 21:20:02 (permalink)
    +1 (1)
    oldtimer
    I have a complete 1989 vintage Hi-Tech Z80 compiler (V4.11). Complete with origional 3 ring binder, hard copy manual and 5.5inch floppy disks.  As far as I can tell this only runs on 32 bit PC's (in a dos box) and won't run even in compatibility mode on a 64 bit system. 

    Something like these? :)

     
     

    Attached Image(s)


    Nearly there...
    #10
    JorgeF
    Super Member
    • Total Posts : 3345
    • Reward points : 0
    • Joined: 2011/07/09 11:56:58
    • Location: PT/EU @ Third rock from the Sun
    • Status: offline
    Re: Hi-Tech Z80 C compiler 2018/09/06 02:41:16 (permalink)
    0
    Hi
     
    The first "Hitech C" compiler I used was on a Sinclair ZX Spectrum 48K.
    After that I only got back to use Hitech tools with the PICs.
     

    Best regards
    Jorge
     
    I'm here http://picforum.ric323.com too!
    And it works better....
    #11
    Jump to:
    © 2021 APG vNext Commercial Version 4.5