• AVR Freaks

PIC32MX695F512L - USB multiple sector read

Author
riese
New Member
  • Total Posts : 7
  • Reward points : 0
  • Joined: 2018/07/27 01:22:52
  • Location: 0
  • Status: offline
2018/09/02 23:59:18 (permalink)
0

PIC32MX695F512L - USB multiple sector read

Hi everyone. I have recently begun my first project with PIC microcontrollers. I try to implement PIC32 as a host to read data fom thumb drives. I am using MLA from 2012 (taken over old project :/ )  with the FSfile system. The maximum speed of read I've managed to have is 165kB/s (bulk transfer with multiple transaction per frame) . My question is - how can I increase the speed? I've heard about multiple sector reading - should I use newer version of MLA to implement this?


Thank you in advance for all answers :)
#1

3 Replies Related Threads

    Mysil
    Super Member
    • Total Posts : 3671
    • Reward points : 0
    • Joined: 2012/07/01 04:19:50
    • Location: Norway
    • Status: offline
    Re: PIC32MX695F512L - USB multiple sector read 2018/09/03 02:05:14 (permalink)
    0
    Hi,
    I think a different version of MLA will not help much.
    MLA for PIC32 was mostly abandoned after v2013-06-15,
    and most of it was discarded in versions after that.
    MDD File System was then v1.4.4
     
    There are several threads in these fora about using FatFs by Elm-Chan to replace the filesystem code in MLA,
    and using DMA for transfer from SD-card.
     
        Mysil
    #2
    riese
    New Member
    • Total Posts : 7
    • Reward points : 0
    • Joined: 2018/07/27 01:22:52
    • Location: 0
    • Status: offline
    Re: PIC32MX695F512L - USB multiple sector read 2018/09/03 06:33:20 (permalink)
    0
    Thank you Mysil :)
    #3
    riese
    New Member
    • Total Posts : 7
    • Reward points : 0
    • Joined: 2018/07/27 01:22:52
    • Location: 0
    • Status: offline
    Re: PIC32MX695F512L - USB multiple sector read 2018/09/11 05:28:53 (permalink)
    0
    I succesfully implemented FatFs, but suprisingly the speed of USB Flash read remained the same (165 KBytes/s) :/ 
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5