• AVR Freaks

Hot!MPLABx v5 - Cannot edit debug watch variables since update??

Page: < 12 Showing page 2 of 2
Author
GeorgePauley
Moderator
  • Total Posts : 1203
  • Reward points : 0
  • Joined: 2009/12/01 13:59:30
  • Location: Chandler AZ
  • Status: offline
Re: MPLABx v5 - Cannot edit debug watch variables since update?? 2019/02/25 09:15:12 (permalink)
-1 (1)
Any chance you can show us your code, and specify a particular variable that is modifiable, and exactly how and when you are attempting to modify it when it fails?  At this point none of us have any idea where to start looking.
#21
AlainV
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2011/04/26 11:18:27
  • Location: 0
  • Status: offline
Re: MPLABx v5 - Cannot edit debug watch variables since update?? 2019/06/17 18:32:20 (permalink)
0
Same for me when using the simulator on a pic18f45k20, I tried to change a few variable to debug, when I use  the F7 to see what happen step by step, I try to change some variable like I did in the past but it wont let me.
I notice this issue with mplabx 5.15 and 5.20.
 
I read the that building in absolut mode could solve the issue but it won't let me used udata_acs
 
What am I doin wrong ?
#22
AlainV
New Member
  • Total Posts : 11
  • Reward points : 0
  • Joined: 2011/04/26 11:18:27
  • Location: 0
  • Status: offline
Re: MPLABx v5 - Cannot edit debug watch variables since update?? 2019/06/22 06:30:51 (permalink)
0
I uninstalled mplabx 5.20 and all prior release and reinstalled 5.20 only and I am still having the same issue.
Whille stepping in the code using F7 I try to change a variable (not a FSR) but when I press enter to confirm the new value, the new value is overwriten by the previous one.
 
Also some value in the variable window are not showing, when I try to modify that value then it shows up with the previous value, I never had issue like that before.
 
Is this a know issue with mplabx or is it something I use the wrong way ?
 
 
#23
GeorgePauley
Moderator
  • Total Posts : 1203
  • Reward points : 0
  • Joined: 2009/12/01 13:59:30
  • Location: Chandler AZ
  • Status: offline
Re: MPLABx v5 - Cannot edit debug watch variables since update?? 2019/06/24 14:16:35 (permalink)
0 (2)
I just saw something... interesting mr green: mr green
I was testing another issue and typing a value into a register in the watch window and it wasn't sticking and I thought:  "That's it!  That's what those guys in the forum are getting on about!" 
 
Turns out I was attempting to enter "ff" and it wouldn't stick.  As soon as I entered "0xff" it did stick.  Maybe that's the issue?
#24
cintet
Super Member
  • Total Posts : 77
  • Reward points : 0
  • Joined: 2007/12/10 09:44:08
  • Location: 0
  • Status: offline
Re: MPLABx v5 - Cannot edit debug watch variables since update?? 2019/11/14 09:24:02 (permalink)
0
MPLABX 5.30, OS Ubuntu 19.10, Device: PIC16HV616. MPLABX Simulator.
I can't change any value of any variable in Watch or Variable Window (Tested in Value, Hex, Decimal, etc, with no luck), just SFR values. 
#25
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5