• AVR Freaks

PLL lock indicator on the PIC32MX274

Author
Wavelength
Super Member
  • Total Posts : 313
  • Reward points : 0
  • Joined: 2012/08/13 08:33:08
  • Location: Cincinnati, Ohio USA
  • Status: offline
2018/08/24 11:30:42 (permalink)
0

PLL lock indicator on the PIC32MX274

Gang,

Trying to get through all these changes going from the MX270 to MX274. In my code for the MX270 I wait for the PLL to lock with this statement:
 
while (! OSCCONbits.SLOCK);
 
I don't see anything that resembles a PLL lock bit in the data sheet for the MX274. There is the SPLLRDY bit in the CLKSTAT register, does that indicate that it's "locked" and ready?
 
Thanks,
Gordon
#1

0 Replies Related Threads

    Jump to:
    © 2021 APG vNext Commercial Version 4.5