Re: HLVD not working with PIC18F4550
2018/08/10 15:45:37
(permalink)
I have hardware which has LCD and push buttons. With push button, I am changing some value and display on the LCD. With HLVD, I am storing the value in the EEprom. So after power restart, the value should be same. But it is not with my program. I have one doubt which I am debugging, the time taken by the EEprom write cycle and Power down time. I am also not able to find out, till what voltage EEprom continue working ? So I keep changing the value of HLVDL.