• AVR Freaks

PIC24 + ENC28J60 simultaneous client and server

Author
cvkumar
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2018/07/26 05:24:30
  • Location: 0
  • Status: offline
2018/07/26 23:14:12 (permalink)
0

PIC24 + ENC28J60 simultaneous client and server

Hi,
I want to use ENC28j60+PIC24 as my module. But my module has to connect one TCP server(say server_IP and port1). And at the same time, the same module should work as a server( of enc_IP and port2), another module will connect to this enc_IP & Port2 as a client. 
Can anyone help me on this how to implement this setup to serve as a server to listen whoever connects and manipulate & as a client to send data to another server?
#1
DarioG
Allmächtig.
  • Total Posts : 54081
  • Reward points : 0
  • Joined: 2006/02/25 08:58:22
  • Location: Oesterreich
  • Status: offline
Re: PIC24 + ENC28J60 simultaneous client and server 2018/07/27 02:37:04 (permalink)
0
Should be doable, even with the "old" TCP/IP stack

GENOVA :D :D ! GODO
#2
Jump to:
© 2020 APG vNext Commercial Version 4.5