• AVR Freaks

Enabling DCache with LWIP_RAW_BASIC_HTTP_EXAMPLE for SAME70Q21 doesn't work

Author
OPriebe
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2018/07/11 04:56:22
  • Location: 0
  • Status: offline
2018/07/12 03:18:43 (permalink)
0

Enabling DCache with LWIP_RAW_BASIC_HTTP_EXAMPLE for SAME70Q21 doesn't work

Hello,

I'm trying to run example project LWIP_RAW_BASIC_HTTP_EXAMPLE for SAME70Q21 with cache enabled:

#define CONF_BOARD_ENABLE_CACHE (in conf_board.h)

As soon as I enable the cache, the HTTP web server included in the example project doesn't work anymore, I don't get access.

I put the GMAC Tx/Rx descriptors into nocache memory section

__attribute__ ((section (".ram_nocache"), aligned (32))) static struct gmac_device gs_gmac_dev;

but with no success.

Do you have any suggestions how to get the project running with cache enabled? I need the cache for my application to speed up data processing.
#1

0 Replies Related Threads

    Jump to:
    © 2019 APG vNext Commercial Version 4.5