• AVR Freaks

RN4871 - Change MAC address permanently

Author
DTFortest
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2018/06/08 05:27:28
  • Location: 0
  • Status: offline
2018/06/11 23:50:44 (permalink)
0

RN4871 - Change MAC address permanently

Hi, 
I'm using RN4871 bluetooth in my project. I change MAC address with & command but after reboot it returns default MAC address. How can I save permanetly a custom MAC address?
#1

1 Reply Related Threads

    AbelR
    New Member
    • Total Posts : 1
    • Reward points : 0
    • Joined: 2018/09/17 04:15:25
    • Location: 0
    • Status: offline
    Re: RN4871 - Change MAC address permanently 2018/10/18 07:00:30 (permalink)
    0
    Hello, it seems there is an undocumented command, "S:,0000,112233445566" and the MAC will be 66:55:44:33:22:11
    #2
    Jump to:
    © 2021 APG vNext Commercial Version 4.5