Hot!Problem using Timer1 on PIC16LF15323

Author
alessandrobertini
New Member
  • Total Posts : 5
  • Reward points : 0
  • Joined: 2015/04/03 05:40:00
  • Location: 0
  • Status: offline
2018/05/25 05:14:03 (permalink)
0

Problem using Timer1 on PIC16LF15323

Hi,
I have a board using a PIC16F15323.
This board is equipped with a relay, a digital input to read, and is configured as i2cbus device slave of another microcontroller.
My board is predominantly in sleep, execpt when timer0 wakes up the micro to read the digital input, or when the host wants to communicate and activates the procedure to set or reset the relay.
My relay is bistable and wants a 5 ms pulse to set or reset its state, so I started the pulse procedure in polling and using timer1 wants to put the board in sleep and finish the pulse procedure at the end of the timer1 period.

The problem is that timer1 doesn't work.

Here is an excerpt of my code :
/*
   Main application
 */
void main(void)
{
   // initialize the device
   SYSTEM_Initialize();
    
    // enable first reset pulse to bistable relay
    RELAY_OPERATE = 1;
    RELAY_STATE = 0;
   
   // Enable the Global Interrupts
   INTERRUPT_GlobalInterruptEnable();

   // Enable the Peripheral Interrupts
   INTERRUPT_PeripheralInterruptEnable();

    // operative loop
   while (1)
   {
        if( RELAY_OPERATE )
        {
            RELAY_OPERATE = 0;        // reset flag
            //
            TMR1_StartTimer();        // handler start relay
        }
        //
        CPUDOZEbits.IDLEN = 0;
        Sleep();                        // put in sleep
      //
      Nop();
   }
}


void interrupt INTERRUPT_InterruptManager (void)
{
    // interrupt handler
    if(PIE0bits.TMR0IE == 1 && PIR0bits.TMR0IF == 1)
    {
        TMR0_ISR();
    }
    //else
    if(INTCONbits.PEIE == 1 && PIE4bits.TMR1IE == 1 && PIR4bits.TMR1IF == 1)
    {
        TMR1_ISR();
    }
    //else
    if(INTCONbits.PEIE == 1 && PIE3bits.SSP1IE == 1 && PIR3bits.SSP1IF == 1)
    {
        I2C1_ISR();
    }
}


void TMR1_Initialize()
{
   //CKPS 1:1; nT1SYNC do_not_synchronize; TMR1ON off; T1RD16 disabled;
   T1CON = 0x04;

   //T1GE disabled; T1GTM disabled; T1GPOL low; T1GGO done; T1GSPM disabled;
   T1GCON = 0x00;

   //GSS T1G_pin;
   T1GATE = 0x00;

   //CS LFINTOSC;
   T1CLK = 0x03;  // 0x04;

   // Clear Interrupt flag before enabling the interrupt
   PIR4bits.TMR1IF = 0;

   // Enabling TMR1 interrupt.
   PIE4bits.TMR1IE = 1;
   
}


void TMR1_StartTimer(void)
{
    if( RELAY_STATE )
    {
        // start relay set pulse
        R_SET_SetHigh();        
    }
    else
    {
        // start relay reset pulse
        R_RESET_SetHigh();        
    }

   // TMR1 stopped
   T1CONbits.TMR1ON = 0;
   
   // TMR1 - 0xFF65 to obtain 5mSec;
   TMR1L = 0x65;
   TMR1H = 0xFF0;
    
   // Clear Interrupt flag before enabling the interrupt
   PIR4bits.TMR1IF = 0;

   // Start TMR1
   T1CONbits.TMR1ON = 1;
}


void TMR1_ISR(void)
{
    if( RELAY_STATE )
    {
        // end relay set pulse
        R_SET_SetLow();
    }
    else
    {
        // end relay reset pulse
        R_RESET_SetLow();
    }

   // Stop TMR1
   T1CONbits.TMR1ON = 0;

   // Clear the TMR1 interrupt flag
   PIR4bits.TMR1IF = 0;
}


void SYSTEM_Initialize(void)
{

    PIN_MANAGER_Initialize();
    OSCILLATOR_Initialize();
    I2C1_Initialize();
    TMR1_Initialize();
    TMR0_Initialize();
}

void OSCILLATOR_Initialize(void)
{
    // NOSC HFINTOSC; NDIV 1;
    OSCCON1 = 0x60;
    // CSWHOLD may proceed;
    OSCCON3 = 0x00;
    // MFOEN disabled; LFOEN disabled; ADOEN disabled; EXTOEN disabled; HFOEN disabled;
    OSCEN = 0x00;
    // HFFRQ 1_MHz;
    OSCFRQ = 0x00;
    // MFOR not ready;
    OSCSTAT = 0x00;
    // HFTUN 0;
    OSCTUNE = 0x00;
}

My problem is that  when the micro executes the following instructions :
   // TMR1 - 0xFF65 to obtain 5mSec;
   TMR1L = 0x65;
   TMR1H = 0xFF0;
the write operation are not executed, timer1 remains with the previous value, and the period between "TMR1_StartTimer" execution and the "TMR1_ISR" activation is about 2 seconds, that is exactly the period of time needed for counting from 0x0000 and the next roll-over with a clock of 31kHz.

Thanks
Alessandro


#1

4 Replies Related Threads

    qɥb
    Monolothic Member
    • Total Posts : 3332
    • Reward points : 0
    • Joined: 2017/09/09 05:07:30
    • Location: Jupiter
    • Status: offline
    Re: Problem using Timer1 on PIC16LF15323 2018/05/25 05:42:06 (permalink)
    0
    I am a bit suspicious of the datasheet.
    It says there is a bit in T1CON called "RD16" documented as
    bit 1 RD16: 16-bit Read/Write Mode Enable bit
    0 = Enables register read/write of Timer1 in two 8-bit operation
    1 = Enables register read/write of Timer1 in one 16-bit operation
     
    but it is not mentioned anywhere else.
    In some other PICs, that is used to enable a latch on the high byte register.
    Just for kicks, try writing TMR1H before TMR1L, and see if it makes a difference.
    Also, change
    TMR1H = 0xFF0;
    to
    TMR1H = 0xFF;

    This forum is mis-configured so it only works correctly if you access it via https protocol.
    The Microchip website links to it using http protocol. Will they ever catch on?
    PicForum "it just works"
    #2
    alessandrobertini
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2015/04/03 05:40:00
    • Location: 0
    • Status: offline
    Re: Problem using Timer1 on PIC16LF15323 2018/05/25 06:27:16 (permalink)
    0
    Hi,
    thank you for reply,
    I followed your suggestions, but the result was the same....
    when i try to write :
    TMR1H = 0xFF
    TMR1L = 0x65
    I continue to watch in my debugger view that TRMR1 value is 0x0000.
     
    Is there someone that has already used timer1 for this PIC?
     
    Alessandro
    #3
    Equinoxin
    New Users
    • Total Posts : 44
    • Reward points : 0
    • Status: offline
    Re: Problem using Timer1 on PIC16LF15323 2018/05/30 14:00:36 (permalink)
    0
    Set RD16 bit as 1.
    In the Timer1 ISR ,you have to reload the timer register values to obtain the required timer delay. 
    Every time you roll over, the timer value needs to be re-initialized.
    I also suggest that you load the timer period values in the TMR1_Initialize() function rather than the TMR1_Start function.
    To reload, or write to the timer, write to the TMR1H first and then to the TMR1L.
     
    #4
    alessandrobertini
    New Member
    • Total Posts : 5
    • Reward points : 0
    • Joined: 2015/04/03 05:40:00
    • Location: 0
    • Status: offline
    Re: Problem using Timer1 on PIC16LF15323 2018/05/31 00:07:29 (permalink)
    0
    I follow your suggestions but timer1 doesn't want to work. Always the same effect.
    sad: sad
     
    #5
    Jump to:
    © 2019 APG vNext Commercial Version 4.5