• AVR Freaks

Hot!MIC4609

Author
MTRGURU
New Member
  • Total Posts : 2
  • Reward points : 0
  • Joined: 2017/09/26 08:58:07
  • Location: 0
  • Status: offline
2018/05/16 08:48:18 (permalink)
0

MIC4609

Hello All
 
I have designed an evaluation board with various modules. On one of the modules for the mosfet drivers I am using the MIC4609 IC. Now the IC seems to work OK until I put any sort of load on it, then the fault pin is pulled down and all the outputs are opened. The datasheet says the causes for the fault is ether a under voltage or over current. So the first thing I check is the supply voltage (12V) with a scope and ensure this does not drop with the fault pin. This turns out to be OK. Now the current pin looked to have a fair amount of motor noise on it, so just to prove concept I just shorted out the low pass cap on the ISNS pin to GND. I am still getting the fault and the bridge's disabling.
 
I have pretty much copied the reference design, but changed the bootstraps to 0.1uF (I am using very low gate charge mosfets), changed the gate resistors to 100Ohm, I only have a single shunt resistor for all three half bridges. I have monitored the current to ensure there are no current spikes (shoot through etc...).
 
I was having problems with very high current draw (and the buck current limiting decreasing the supply voltage below the threshold causing a fault). But once I put the reverse diodes on the gates this seemed to cure the problem and the supply voltage is now stable.
 
Does anyone have any idea (of have any good opinions) on what else could be causing the fault?
 
Thanks
#1

2 Replies Related Threads

    t1d
    Senior Member
    • Total Posts : 144
    • Reward points : 0
    • Joined: 2015/01/26 15:49:24
    • Location: 0
    • Status: offline
    Re: MIC4609 2018/08/11 01:29:59 (permalink)
    0
    I know this is old, but I am having a similar problem with my DIY DC Electronic Load project. An op amp controls five mosfets. The operations are correct, from 0 to 0.5 volts, then the mosfets seem to go full throttle and the current limit, on the PSU, gets pegged.  Did you ever determine what your issue was? Thanks.
    #2
    _dex
    Junior Member
    • Total Posts : 117
    • Reward points : 0
    • Joined: 2008/03/19 13:57:34
    • Location: 0
    • Status: offline
    Re: MIC4609 2020/08/03 02:42:08 (permalink)
    4 (1)
    What has happened actually with this driver? Currently there is no any result from microchip site, the only one 3Phase driver is 4607 which is marked as not recommended for new design.
     
    4609 was quite similar to IR2130. Is it not produced anymore?
     

    But once I put the reverse diodes on the gates this seemed to cure the problem and the supply voltage is now stable.

    Was that not due to layout problem? If the diode on gates solved the problem it seems like track inductance problem. High gates current could produce high negative undershoots and then in effect IC ground is floating.
     
    There are very good ANs from IR how to make proper layout for such drivers, look for IR2130 AN.
    post edited by _dex - 2020/08/03 02:46:05
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5