• AVR Freaks

SST26VF032 write issue

Page: < 12 Showing page 2 of 2
Author
BumpSplat
Senior Member
  • Total Posts : 163
  • Reward points : 0
  • Joined: 2017/11/06 13:23:11
  • Location: Bend, OR
  • Status: offline
Re: SST26VF032 write issue 2018/10/07 16:21:41 (permalink)
0
Seeing very strange behavior.... Is a reset is required after an erase cycle?  Also, the reset sequence uses an 8 bit "reset enable" CSHigh slight delay CSLow 8 bit "reset".  I'm using SPI in 16 bit mode. 
- Do I need to change my SPI interface to 8 bit for the reset process? -Thanks
- Is it possible to very a software reset was completed correctly?  It's very strange I can successfully program the IC 7 times and it fails on the eighth cycle.  It's actually random but the concept is the same....


-T
 
#21
BumpSplat
Senior Member
  • Total Posts : 163
  • Reward points : 0
  • Joined: 2017/11/06 13:23:11
  • Location: Bend, OR
  • Status: offline
Re: SST26VF032 write issue 2018/10/17 13:15:02 (permalink)
0
Closure -
The issue has been tracked back to the PCB coupling signals through a poor power plane.  Also, 8 bit commands appear to be working fine using a 16bit word or 8bit command byte. :)
 
Tim
#22
Page: < 12 Showing page 2 of 2
Jump to:
© 2020 APG vNext Commercial Version 4.5