• AVR Freaks

Stuck on Loading

Author
MitYeltu
Senior Member
  • Total Posts : 129
  • Reward points : 0
  • Joined: 2010/02/02 12:05:03
  • Location: TN
  • Status: offline
2018/04/12 04:58:19 (permalink)
0

Stuck on Loading

This is my first time trying MPLAB Express. I am familiar with MPLAB, but have never used the cloud based version. I have tried several timed to get the software to load, but it hangs every time I try at the same point. Even right now the wheel is spinning at "Loading device information". It has been doing this now for about 5 minutes. This is the 3rd time I have tried today and waited to see what - if anything - happens.
 
Am I doing something wrong? I log in and it does a couple of things and then hangs on "Loading device information". I don't have a device connected, I have no specified a device anywhere, I have not created a project anywhere, so I don't really understand what device information its trying to load.
 
Does anyone have any suggestions on what I should try?
#1

3 Replies Related Threads

    MitYeltu
    Senior Member
    • Total Posts : 129
    • Reward points : 0
    • Joined: 2010/02/02 12:05:03
    • Location: TN
    • Status: offline
    Re: Stuck on Loading 2018/04/16 04:13:11 (permalink)
    0
    Well, don't everybody chime in at once....
    #2
    NeDDRaG
    New Member
    • Total Posts : 0
    • Reward points : 0
    • Joined: 2018/06/08 13:28:53
    • Location: 0
    • Status: offline
    ➥ Approval Pending
    Re: Stuck on Loading 2018/06/18 03:15:53 (permalink)
    #3
    arcs_n_sparks
    New Member
    • Total Posts : 7
    • Reward points : 0
    • Joined: 2006/11/16 13:32:32
    • Location: 0
    • Status: offline
    Re: Stuck on Loading 2018/10/29 04:23:06 (permalink)
    0
    MitYeltu,
     
    I tried MP express for the first time today (long time MPLAB X IDE user). Same problem; hangs at "Loading Device Information." This is using Internet Explorer, since the Java plug-in is not supported in Chrome or Edge. I cannot find a solution to this either.
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5