• AVR Freaks

AnsweredHot!IPE Command Line (ipecmd) suppress log files?

Author
KTrenholm
Super Member
  • Total Posts : 865
  • Reward points : 0
  • Joined: 2012/08/08 14:04:23
  • Location: Connecticut, USA
  • Status: offline
2018/04/06 09:27:02 (permalink)
0

IPE Command Line (ipecmd) suppress log files?

Hey all,
 
I'm currently putting together a windows batch file for use in a production environment to program a device via the ipe command line (ipecmd.jar).
 
I'm writing the device no problem, but every time I run the command I end up with 5 log files:
log.0
log.1
log.2
MPLABXLog.xml
MPLABXLog.xml.lck
 
Is anybody aware if there is a way to suppress these logs?  The Readme for IPECMD.htm file doesn't seem to mention these log files at all, let alone how to suppress them.  This could be a potential issue with our production machines, as they will be running the batch file from a network location, and do not have write permissions for the directory from which these batch files will be run.  I would imagine this would throw an error message, although I haven't tested this on one of the production machines yet.  It would be ideal to just be able to suppress them.
 
Appreciate any tips/tricks if anyone out there has 'em.
#1
mmujumdar
Starting Member
  • Total Posts : 13
  • Reward points : 0
  • Joined: 2018/04/23 16:27:06
  • Location: 0
  • Status: offline
Re: IPE Command Line (ipecmd) suppress log files? 2018/04/25 11:19:21 (permalink) ☼ Best Answerby KTrenholm 2018/04/26 08:56:00
5 (1)
MPLAB IPE User's Guide http://ww1.microchip.com/downloads/en/DeviceDoc/50002227C.pdf provides information on suppressing the log files. This requires the user to log in using the Advanced Mode (Settings -> Advanced Mode, as shown in Figure 2-5 of the User's Guide). In Advanced Mode, the Settings section gives the user control to select the desired  message logging level (more information available in the section on Diagnostics, TABLE 2-6 of the User's Guide). Setting the logging level to OFF suppresses the log files.
#2
KTrenholm
Super Member
  • Total Posts : 865
  • Reward points : 0
  • Joined: 2012/08/08 14:04:23
  • Location: Connecticut, USA
  • Status: offline
Re: IPE Command Line (ipecmd) suppress log files? 2018/04/26 08:55:55 (permalink)
0
Hey, thanks!
#3
ajmac01
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2021/02/19 11:02:00
  • Location: 0
  • Status: offline
Re: IPE Command Line (ipecmd) suppress log files? 2021/02/25 14:30:03 (permalink)
4 (1)
Is there a way to suppress logs through the command line?
#4
tech24x7
Junior Member
  • Total Posts : 113
  • Reward points : 0
  • Joined: 2013/10/14 21:38:52
  • Location: 0
  • Status: offline
Re: IPE Command Line (ipecmd) suppress log files? 2021/03/03 05:55:36 (permalink)
4 (1)
OS<Type>
Special Memory Setting
Type:
L<Level 0..7><Path> = Enable Diagnostics Log
[0=OFF, 1=SEVERE, 2=WARNING, 3=INFO, 4=CONFIG, 5=FINE, 6=FINER, 7=FINEST]
  
Be default it is off, still you can use -OSL0 switch to off log messages.
#5
Jump to:
© 2021 APG vNext Commercial Version 4.5