• AVR Freaks

Hot!Harmony, MSD and USB 3.0 Thumb Drives

Author
NKurzman
A Guy on the Net
  • Total Posts : 18141
  • Reward points : 0
  • Joined: 2008/01/16 19:33:48
  • Location: 0
  • Status: offline
2018/03/05 20:37:23 (permalink)
0

Harmony, MSD and USB 3.0 Thumb Drives

I am told that there is an issue with Harmony V 1.11 and USB 3.0 Memory Sticks.  
Has anyone seen this.
What about in Harmony 2.XX?
#1

2 Replies Related Threads

    weehau
    Starting Member
    • Total Posts : 51
    • Reward points : 0
    • Joined: 2010/03/28 02:10:50
    • Location: 0
    • Status: offline
    Re: Harmony, MSD and USB 3.0 Thumb Drives 2020/01/14 23:16:46 (permalink)
    0
    I am facing the same issue in harmony v2_06. The PIC32MZ running on Mchp harmony USB MSD Host library failed to enumerate a USB 3.0 pen drive. 
    #2
    NKurzman
    A Guy on the Net
    • Total Posts : 18141
    • Reward points : 0
    • Joined: 2008/01/16 19:33:48
    • Location: 0
    • Status: offline
    Re: Harmony, MSD and USB 3.0 Thumb Drives 2020/01/15 07:04:37 (permalink)
    5 (2)
    I just got an up dated driver from microchip.
    This appears to fix the issue with Sticks not enumerating.
    I am not sure the issue was a 3.0 issue.
    I will ask if I can post their fix.
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5