• AVR Freaks

Hot!Need to load the program without removing the IC from the circuit board

Page: < 12 Showing page 2 of 2
Author
NorthGuy
Super Member
  • Total Posts : 5578
  • Reward points : 0
  • Joined: 2014/02/23 14:23:23
  • Location: Northern Canada
  • Status: online
Re: Need to load the program without removing the IC from the circuit board 2019/02/24 11:40:40 (permalink)
0
john_ive
Between tapping from 10K resistor and capacitor and to PIC's reset pin..?

 
Yes, I posted the link on the schemtics.
 
john_ive
Is resistor is 470R or 4.7K..?
Pic datasheet recommended 470R resistor...



I recommend 4.7K for these PICs.
 
#21
john_ive
Super Member
  • Total Posts : 204
  • Reward points : 0
  • Joined: 2017/05/22 22:22:08
  • Location: 0
  • Status: offline
Re: Need to load the program without removing the IC from the circuit board 2019/02/27 04:39:55 (permalink)
0
I'm using PICKIT 2 for loading the program in PIC controller.
While creating a new project from existing file,MPLAB X IDE window appering like this.
 
In this which one have to choose "ONLY PICKIT or SN:OIHoss"..?
I'm using PIC18F4520 controller.

Attached Image(s)

#22
jack@kksound
code tags!
  • Total Posts : 3203
  • Reward points : 0
  • Joined: 2014/05/14 10:03:19
  • Location: 0
  • Status: offline
Re: Need to load the program without removing the IC from the circuit board 2019/02/27 11:10:22 (permalink)
+1 (1)
The two options are the same, the first selects the "default" pickit2 and the second is simply the serial number/"name" of the attached pickit2(s). If you had more then one attached you would (should) see them all listed here. With only one listed pick either name, it should work.
#23
oliverb
Super Member
  • Total Posts : 206
  • Reward points : 0
  • Joined: 2009/02/16 13:12:38
  • Location: 0
  • Status: offline
Re: Need to load the program without removing the IC from the circuit board 2019/07/22 07:55:04 (permalink)
0
FWIW historically it was common to use a RC reset pulse, but with most PIC models now you should be able to pull MCLR up with 10K and no capacitor, and just rely on the power up timer and/or brown-out detection to generate a reliable reset.
PICkit3 demo boards appear to have 10K on MCLR, tacked onto the programming connector.
 
#24
Page: < 12 Showing page 2 of 2
Jump to:
© 2019 APG vNext Commercial Version 4.5