• AVR Freaks

Can Bus Connection with the Can Bus Analyzer with C#

Author
pad94
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2018/01/18 07:01:18
  • Location: 0
  • Status: offline
2018/01/19 00:31:35 (permalink)
0

Can Bus Connection with the Can Bus Analyzer with C#

Hello Guys,
 
i wanted to develope a Application with C# and not with C++. Now my question is, is it possible to read the Data sent from the Microchip Can Bus Analyzer? I just want to read the Data and the ID from the Can Bus. I dont even need more.
 
Thanks for your Answers.
Greetings Patrick
#1

3 Replies Related Threads

    ccandido
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2010/01/05 12:58:59
    • Location: 0
    • Status: offline
    Re: Can Bus Connection with the Can Bus Analyzer with C# 2019/09/15 17:52:42 (permalink)
    0
    Hi pad94,
    I have it question,
    I have c# driver WinUsb ok,
    I need function driver usb, and commands list to send and receiver pip.
     
    1- usb drive or lib.
    2- list commands.
    others we developper custom code.
     
    thanks,
    Carlos.
    #2
    ccandido
    New Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2010/01/05 12:58:59
    • Location: 0
    • Status: offline
    Re: Can Bus Connection with the Can Bus Analyzer with C# 2019/09/15 17:52:42 (permalink)
    0
    Hi pad94,
    I have it question,
    I have c# driver WinUsb ok,
    I need function driver usb, and commands list to send and receiver pip.
     
    1- usb drive or lib.
    2- list commands.
    others we developper custom code.
     
    thanks,
    Carlos.
    #3
    Lurch
    Super Member
    • Total Posts : 646
    • Reward points : 0
    • Joined: 2010/08/04 14:05:04
    • Location: 0
    • Status: offline
    Re: Can Bus Connection with the Can Bus Analyzer with C# 2019/09/16 10:37:40 (permalink)
    0
    Download the Visual Studio source for the Can Bus Analyzer from MCHP and look at the code. It's just a bulk USB connection. If you send the right code, it will send the data in the record format listed in globals.h
    Changing from Visual Studio C++ to C# shouldn't be a problem.
    #4
    Jump to:
    © 2021 APG vNext Commercial Version 4.5