• AVR Freaks

Helpful ReplyHow to draw a filled circle with ARIA

Author
epareja
Super Member
  • Total Posts : 380
  • Reward points : 0
  • Joined: 2003/11/07 12:53:08
  • Location: Colombia
  • Status: offline
2017/12/26 00:20:29 (permalink)
0

How to draw a filled circle with ARIA

Hello,
is there a way to draw a filled circle but only inside the circle and not all the squared base?


Ernesto Pareja J
www.dcctrains.netne.net

#1
MikeinAZ
Administrator
  • Total Posts : 321
  • Reward points : 0
  • Joined: 2014/06/03 07:25:32
  • Location: Chandler, AZ
  • Status: offline
Re: How to draw a filled circle with ARIA 2018/01/02 10:01:23 (permalink) ☄ Helpfulby epareja 2018/01/02 10:11:38
0
Hello,
 
The short answer for you is currently no, we do not have circle fill available in Harmony v2.05.
 
A reasonable work around is for you to use a picture object, which will effectively display the same thing.
 
In Harmony v2.06, we already have an entirely new widget for drawing circles, filled arcs and using them for some meter functions.  However the release of this is at least a couple of months away.  
#2
epareja
Super Member
  • Total Posts : 380
  • Reward points : 0
  • Joined: 2003/11/07 12:53:08
  • Location: Colombia
  • Status: offline
Re: How to draw a filled circle with ARIA 2018/01/02 10:12:55 (permalink)
0
Thank you Mike!
 
I already did that using an image widget.
Glad to know the new widgets are coming. 
 


Ernesto Pareja J
www.dcctrains.netne.net

#3
gemini11
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2015/01/12 19:26:34
  • Location: 0
  • Status: offline
Re: How to draw a filled circle with ARIA 2018/11/03 16:04:27 (permalink)
0
So now that V2.06 of Harmony is out, how do you do a filled circle or rectangle?
#4
Ed@Microchip
Super Member
  • Total Posts : 160
  • Reward points : 0
  • Joined: 2017/04/06 09:39:29
  • Location: 0
  • Status: offline
Re: How to draw a filled circle with ARIA 2018/11/07 09:15:56 (permalink)
0
gemini11
So now that V2.06 of Harmony is out, how do you do a filled circle or rectangle?


In v2.06:
To draw a filled circle, use the Arc drawing widget. Set the thickness = radius and center angle to 360, and it will draw a filled circle.
To draw a filled rectangle, use a panel widget.
 
In the next release v2.07, the Circle and Rectangle widgets will have built-in thickness/fill properties.
#5
Jump to:
© 2020 APG vNext Commercial Version 4.5