• AVR Freaks

Hot!Blank web page after using MPFS generator on Harmony web_server_nvm_mpfs sample project

Author
WmDrago
New Member
  • Total Posts : 17
  • Reward points : 0
  • Joined: 2017/12/05 15:01:45
  • Location: 0
  • Status: offline
2017/12/14 12:51:58 (permalink)
0

Blank web page after using MPFS generator on Harmony web_server_nvm_mpfs sample project

All,
 
I built and loaded the web_server_nvm_mpfs project and see a very nice web page on the client computer's browser. As part of my learning process I tried compileing the web source with the MPFS Generator. After clean/rebuild/load I get just a blank screen in the web browser. I noticed that the mpfs_img2.c file MPFS Generator creates is slightly different than the one supplied with the project.
 
Elsewhere in these forums I saw a post that suggested there is a bug in the MPFS Generator v2.34, and that v2.33 should used instead. Is this true? If so, where can I download v2.33?
 
Thanks...
 
Windows 7/MPLAB X v4.05/Harmony V2.04/MPFS Generator v2.34/PIC32MZ2048EFH144 Starter Kit/Java JRE 1.8.0_151
#1

3 Replies Related Threads

    Bruce95
    Starting Member
    • Total Posts : 2
    • Reward points : 0
    • Joined: 2015/03/06 14:33:38
    • Location: 0
    • Status: offline
    Re: Blank web page after using MPFS generator on Harmony web_server_nvm_mpfs sample projec 2017/12/20 07:37:11 (permalink)
    5 (2)
    I ran in to the same issue.  Version 2.33 works for me.  I attached the one from Harmony v1.10.
    #2
    WmDrago
    New Member
    • Total Posts : 17
    • Reward points : 0
    • Joined: 2017/12/05 15:01:45
    • Location: 0
    • Status: offline
    Re: Blank web page after using MPFS generator on Harmony web_server_nvm_mpfs sample projec 2017/12/20 10:04:40 (permalink)
    0
    Fantastic. Thank you!
    #3
    Soren.Bang
    Starting Member
    • Total Posts : 47
    • Reward points : 0
    • Joined: 2012/10/10 13:01:51
    • Location: Denmark
    • Status: offline
    Re: Blank web page after using MPFS generator on Harmony web_server_nvm_mpfs sample projec 2019/10/23 10:50:19 (permalink)
    0
    Thank you, thank you, thank you - I was just about going nuts - My harmony 2.06 project now works as it should using the mpfs generator version 2.33 (from Harmony 1.10).
     
    Regards
    Søren
    #4
    Jump to:
    © 2020 APG vNext Commercial Version 4.5