Helpful ReplyHot!Solved write into FLASH and read on PIC32MM

Author
Witek_Polska
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/10/30 08:34:58
  • Location: 0
  • Status: offline
2017/11/30 02:15:36 (permalink)
0

Solved write into FLASH and read on PIC32MM

I have got problem with writing into flash memory  . I changed code in original http://ww1.microchip.com/downloads/en/DeviceDoc/60001121g.pdf
and now it's ok:
 
#1
Witek_Polska
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/10/30 08:34:58
  • Location: 0
  • Status: offline
Re: Solved write into FLASH and read on PIC32MM 2017/11/30 02:23:08 (permalink)
0
I can't add source because is always problem!
#2
kc4ydx
New Member
  • Total Posts : 6
  • Reward points : 0
  • Joined: 2017/10/25 15:19:37
  • Location: 0
  • Status: offline
Re: Solved write into FLASH and read on PIC32MM 2017/12/06 17:20:55 (permalink) ☄ Helpfulby YG 2018/04/24 00:40:31
5 (1)
I've attached an example of a working PIC32MM flash writing code. Its based off of the Microchip example code.
Hope this helps someone get started working with flash.
 
Rename flash.txt to flash.h
 
#3
Witek_Polska
New Member
  • Total Posts : 10
  • Reward points : 0
  • Joined: 2017/10/30 08:34:58
  • Location: 0
  • Status: offline
Re: Solved write into FLASH and read on PIC32MM 2017/12/07 08:49:48 (permalink)
0
Thanks , but i couldn't add code due to forum problem , I solved this problem on PIC32mm and i was going to show on forum but every time I would add code then was blocked.
 
#4
Jump to:
© 2018 APG vNext Commercial Version 4.5