• AVR Freaks

Hot!ESP8266 vs ATWINC1500 Which one is easier to use?

Author
chipmonk
Starting Member
  • Total Posts : 43
  • Reward points : 0
  • Joined: 2012/01/23 07:20:30
  • Location: 0
  • Status: offline
2017/11/20 08:00:23 (permalink)
0

ESP8266 vs ATWINC1500 Which one is easier to use?

Hi, 
 
I have an application that needs to read and write to Firebase, I already set up my database and its easy to get data from firebase example - 'https://[PROJECT_ID].firebaseio.com/users/jack/name.json' - gets data for me. This is not a complex application, I dont want to make it complicated, can anyone assist? 
 
Which module must I use and are there any simple commands to connect to a WIFI network then just read adn write data I need.
#1

2 Replies Related Threads

    concertinaman
    Bug Sorter
    • Total Posts : 248
    • Reward points : 0
    • Joined: 2007/06/14 05:56:58
    • Location: UK
    • Status: offline
    Re: ESP8266 vs ATWINC1500 Which one is easier to use? 2017/11/21 03:21:48 (permalink)
    0
    For me, the low cost of the ESP8266 and the need for a host processor for the ATWINC1500 would make this a no-brainer, though in practice, these days I'd probably start with the ESP32 for anything WIFI.
    #2
    jyaron
    Super Member
    • Total Posts : 392
    • Reward points : 0
    • Joined: 2003/11/07 12:43:15
    • Status: offline
    Re: ESP8266 vs ATWINC1500 Which one is easier to use? 2019/04/16 16:03:33 (permalink)
    #3
    Jump to:
    © 2019 APG vNext Commercial Version 4.5