Hot!MCC Bootloader Generator reverses Priority Interrupt Vectors

Author
GrahamH
Starting Member
  • Total Posts : 88
  • Reward points : 0
  • Joined: 2010/04/23 20:37:12
  • Location: Austin, TX
  • Status: offline
2017/11/13 15:54:47 (permalink)
0

MCC Bootloader Generator reverses Priority Interrupt Vectors

Windows 10 (Current)
MPLAB-X 4.05
Compiler XC-8 Version 1.4.4
Target MCU: PIC18F25K22
MCC 3.36
Bootloader Generator version 2.2.0
Using an application code address offset of 0x800
Bootloader Generator generates bootloader code with High Priority and
Low Priority Vectors reversed.
In file "pic18f_bootload.c"

Attached Image(s)

#1

4 Replies Related Threads

    alecdavis
    Starting Member
    • Total Posts : 18
    • Reward points : 0
    • Joined: 2016/11/03 16:34:31
    • Location: 0
    • Status: offline
    Re: MCC Bootloader Generator reverses Priority Interrupt Vectors 2017/11/13 23:23:21 (permalink)
    0
    Already reported http://www.microchip.com/forums/m962133.aspx
     
    I thought it had been sorted.
    #2
    GrahamH
    Starting Member
    • Total Posts : 88
    • Reward points : 0
    • Joined: 2010/04/23 20:37:12
    • Location: Austin, TX
    • Status: offline
    Re: MCC Bootloader Generator reverses Priority Interrupt Vectors 2017/11/14 10:43:37 (permalink)
    0
    Hmmmm.
     
    I guess in the future, I need to set the default search time limits much further back.
     
    It has been over 11 months since that report.
     
    They are still including Bootloader version 2.2.0 in the current MCC, so nothing has been fixed in a year.
     
    --- Graham
     
    ==
    #3
    Danno
    Super Member
    • Total Posts : 202
    • Reward points : 0
    • Joined: 2005/09/07 10:12:10
    • Status: offline
    Re: MCC Bootloader Generator reverses Priority Interrupt Vectors 2017/11/14 14:27:32 (permalink)
    0
    This and many other bugs have been fixed but awaiting release which should be imminent.
    #4
    Danno
    Super Member
    • Total Posts : 202
    • Reward points : 0
    • Joined: 2005/09/07 10:12:10
    • Status: offline
    Re: MCC Bootloader Generator reverses Priority Interrupt Vectors 2018/01/18 12:52:42 (permalink)
    0
    The new release is Available.  https://www.microchip.com/mcc.  Go to the "Current Download" tab, note 8 bit bootloader is now at release 2.2.31.
     
    #5
    Jump to:
    © 2018 APG vNext Commercial Version 4.5