• AVR Freaks

Curiosity Board Issue: Could not connect to tool hardware: PKOBSKDEPlatformTool

Author
kenneth.daniels@snet.net
New Member
  • Total Posts : 1
  • Reward points : 0
  • Joined: 2017/09/10 05:09:54
  • Location: 0
  • Status: offline
2017/09/13 02:15:10 (permalink)
0

Curiosity Board Issue: Could not connect to tool hardware: PKOBSKDEPlatformTool

Hi All,
 
Purchased the Curiosity dev board.
 
I installed MPLAB-X-IDE on my mac, and tried debugging the board with sample code from web site.
 
I get the following:
 
Could not connect to tool hardware: PKOBSKDEPlatformTool, com.microchip.mplab.mdbcore.pkobskde.PKOBSKDEDbgToolManager
The debugger could not be started.  Terminating debug session.

 
 
What is real interesting, thinking it might be a Mac issue, I then went and installed the same set of tools on the a Windows 8 notebook I have, and I get the same issue.
 
I definitely see the Curiosity board as an option on the select platform debug menu, and option goes away when USB unplugged.
 
Any thoughts?.   Never had this much trouble getting started.
 
#1

2 Replies Related Threads

    Martin
    New Member
    • Total Posts : 9
    • Reward points : 0
    • Joined: 2010/06/29 12:12:01
    • Location: 0
    • Status: offline
    Re: Curiosity Board Issue: Could not connect to tool hardware: PKOBSKDEPlatformTool 2019/05/26 12:42:10 (permalink)
    +1 (1)
    Hello,
    I have the same problem with my 'PIC32MM USB Curiosity Development Board'
     
    The programmer could not be started: Could not connect to tool hardware: PKOBSKDEPlatformTool, com.microchip.mplab.mdbcore.pkobskde.PKOBSKDEDbgToolManager
     
    Is any solution for that?
    #2
    stenakew
    Starting Member
    • Total Posts : 34
    • Reward points : 0
    • Joined: 2013/09/04 10:54:16
    • Location: 0
    • Status: offline
    Re: Curiosity Board Issue: Could not connect to tool hardware: PKOBSKDEPlatformTool 2019/05/28 00:06:16 (permalink)
    0
    Hej.
    Assuming "Curiosity" means 8 bit with 20pin socket (DM164137) in post #1.
    Using MPLAB-X 5.20 on Mac OS 10.14.4:
    No problem loading/debugging a small program with a PIC16F1509 on the Curiosity board.
     
    /Sten-Åke
    #3
    Jump to:
    © 2020 APG vNext Commercial Version 4.5