• AVR Freaks

RN4871 is not connecting

Author
vigneshkumarp14
New Member
  • Total Posts : 4
  • Reward points : 0
  • Joined: 2017/07/12 03:39:09
  • Location: 0
  • Status: offline
2017/08/20 21:26:06 (permalink)
0

RN4871 is not connecting

Hi, I'm developing a project to send data from an android app to a target board(microcontroller) using bluetooth. Initially we bought a module from microchip named RN4020 and its working fine with our own developed android app which can able to send and receive data with microcontroller. As suggested from microchip we bought RN4871 module. But the android app was not able to read atleast the RN4871modules BLUETOOTH SERVICE and CHARACTERISTICS. To send/receive data the BLUETOOTH SERVICE and CHARACTERISTICS is necessary, but I cant able to read those things. Also RN4871 fails the same with other android app available in play store. An LED is used to denote the connection status which will blink for every second(approximately) in RN4871, at the time of connecting it blinks twice but after some time it comes to normal blinking state. I need some suggestion from microchip to follow the project further. 
 
Thanks.
#1
Jump to:
© 2021 APG vNext Commercial Version 4.5